The gauge reports small currents (< DeadBand) as 0mA but they are still being used to calculate capacity parameters (RemCap, SOC, etc.). The smaller the current, the longer it takes to have a noticeable effect on these parameters (can be hours or days…
Other Parts Discussed in Thread: BQ27210 Dear all,
we are using the BQ27210 in a project.
we are facing some calibration issues.
I couldn't find elaborated data on what is the best way to calibrate this system. we still see some differences in reading…
Other Parts Discussed in Thread: BQ27210 , BQ27200 , BQ27000 Dear all,
I'm using the BQ27210 , and also the NRND bq27200 (because of legacy production we cannot replace).
I saw that there is "Test System for BQ27000 BQ27200 Based Circuit Boards"…
Other Parts Discussed in Thread: BQ27210 Hi
I'm usign the BQ27210 to monitor the battery charge of a custom device we're developing, but we're having some problems related to the BQ27210 operation. According to the datasheet, I can see the following expected…
Other Parts Discussed in Thread: BQ27210 Hi,
We have to use a battery gas gauge for our product. But our batteries are charged with an external charger.
We think used a Bq27210, what's happened if we unplug batteries to charged them and plug.
Does…
Other Parts Discussed in Thread: BQ27210 , BQ27500 Hi
we are using TI BQ27210 in our project for Battery voltage monitoring purpose.we are using the default driver bq27x00_battery .c provided with Android JB4.3.we are able to read the entries from the battery…
Hi
Just a silly question? How do you do to read the INIT bit? Can I read directly the MODE register? Or must I write int CTRL register the command before reading mode? Just I want to be sure I'm doing this correctly.
Thanks in advance.
Eduardo …