Part Number: MSP430FR2676 Other Parts Discussed in Thread: MSP430FR2632 I was browsing around TI's website and I happened upon Captivate EMC.
https://www.ti.com/lit/wp/slay045b/slay045b.pdf
https://www.ti.com/tool/CAPTIVATE-EMC
At first, I thought…
Here it is:
#include "CAPT_UserConfig.h"
//*****************************************************************************
//
//! Captivate Element Definitions
//! All elements in this application are defined below.
//! Each element has 3 components…
Part Number: EVM430-CAPMINI Other Parts Discussed in Thread: MSP430FR2512 , ENERGYTRACE I want to make a 4-20mA loop powered picofard capacitance meter with adjust able offset (upto 100pF) with a full scale range adjustable up to probably upto 10pF. It…
Hello James,
Thank you for reply.
James Evans said: When you say the issue doesn't happen when UPS is removed, do you mean that the AC-to-DC is plugged into a wall outlet with AC mains?
- yes, it was connected to AC mains.
Meanwhile we are…
Piocky,
For calibration, you actually want the interaction with the CapTIvate Design center. So you need that I2C HID Bridge connection. The SBW connections are utilized for programming the MSP430.
The type of isolators you linked are really good for…
Hello Eddi,
We connect our device to the CAPTIVATE-PGMR PCB. We were able to reproduce the Error in this environment. What we can see is that the LTA value in the Error case is very unstable (between 2100 and 1900) where else in the cases where the…
Hi, Robert,
The capcitive touch in MSP430FR4133 is designed with pin-oscillation theory. The capacitive touch in MSP430FR2512 is designed with high-performance charge-transfer CapTIvate technology. The CapTIvate technology has better performance than pin…
Part Number: MSP430FR2522 Hello,
Regarding to RF Susceptibility(EMC test) on MSP430FR2522, my customer is asking some question.
They have tested RF conduction noise test but it had made false detection at around 2MHz noise input.
The sensor mode is self…
Part Number: MSP430FR2633 Other Parts Discussed in Thread: CAPTIVATE-PHONE , Hello,
I am using MSP430FR2633 TSSOP package controller for 16 elements keypad sensor for touchpad. I am using mutual capacitance technology for this purpose. I have followed…