Hi RD,
Please try issuing a software reset after startup to the broadcast address . This should reinitialize all devices even if there are duplicate addresses.
Thanks,
Paul
Part Number: CC2650EM-7ID-RD Other Parts Discussed in Thread: CC2650 Tool/software: Code Composer Studio Hi, there:
The application is based on the example project, Simple_broadcaster. And it is setup as BLE broadcasting only at the frequency of 10Hz.…
Other Parts Discussed in Thread: CC2543 Hi Experts,
My customer is working on the CC2543 design for a remote controller. We use the miniLE stack and the scenario is that when button pressed, we send out broadcast packets, then:
1. We would want to close…
Part Number: CC1101 Other Parts Discussed in Thread: CC1310 , LAUNCHXL-CC1310
Hi, I'm trying to communicate a LAUNCHXL-CC1310 board with a custom board which uses a CC1101. I'm using the custom board on a proyect based on MPLAB, on the other hand I…
Hi Tejas P R,
Yes, we have the internal current source pull up, and the current source will be determined by the 1.5A or 3A current broadcast.
For example, when you insert the Rd(5.1kohm) in the CC1, and you use the CHG=1, CHG_HI=0, choose the 1.5A…
Hello Greenja,
The software example is now available on the CC2543 product folder ( http://www.ti.com/lit/zip/swrc291 ). This is meant to be an example that the users can use a reference and modify to their needs. It is possible to create a much simpler…
Part Number: CC2652RB EXT_EP-10846 details note that the issue is rare and is seen when device is disconnected/connected by walking away. The details also note that the issue was seen in "Central + Broadcasting" mode. I have been seeing a similar…
Part Number: TDA4VEN-Q1 Tool/software: Dear Ti,
OS: Linux+RTOS(J722S)
PSDK : ti-processor-sdk-rtos-j722s-evm-09_02_00_05
Ser/Deserializer : UB953/UB960
We tried to use the imx390 driver in the sdk package to light up the camera, but it didn't go well…
Hi Rahul ,
,In our datasheet
we are using pru-eth0 and pru-eth1 .
some queary reading this
1)Is dps83822 driver required and also cpsw and emac driver ?
2) currently status is eth0 and eth1 showing in os , it is required to program PRU-ICCS?
I am attached…
Part Number: CC2531USB-RD Other Parts Discussed in Thread: CC2531 I am currently using Packet sniffer(2.18.0) with CC2531 USB dongle. I can check broadcast messages. However, i can't capture the unicast messages. I wonder if it's possible to capture the…