Part Number: LMX2572 Tool/software: I'm entering reference clock phase noise with the use Points options. WHen I do that, the interpolation/extrapolation is very off, with a system level phase noise of +20 dBm and some very odd looking traces at lower…
Part Number: CC3301 Tool/software: Hi TI Experts, We are developing a custom hardware of gateway using CC3301.We are facing an issue with channel power measurement. We are getting the channel power more than expected. Please see the following image. …
Part Number: OPA380 Other Parts Discussed in Thread: OPA859 Tool/software: Hi Sir,
may we know two quesiton, and learn from you,
1. According to the reference circuit on page 11 of the datasheet, with VBIAS set to 250 mV, the output signal swing is…
Hi,
We have not developed or tested this beyond the information Richard shared in the thread you linked. As mentioned, the 433 MHz-band is typically more utilised at lower power levels as +20 dBm is not allowed in most regions, so we have not spent…
Hi,
Please follow the steps outlined in the following thread (roughly, modify categories.xml and add the PHY settings files as described): https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1448869/cc1314r10…
Hi Albin,
The 2.4 GHz, +10 dBm design cannot exceed +10 dBm due to using a VDDR bias.
For the 2.4 GHz, +20 dBm design - that is supplied with VDDS. However, when the device is not in saturation (i.e. lower PA gain settings) the device-to-device…
Hi,
I see you are using the CC2652P device. If you are using it in the +20 dBm configuration, where the PA is supplied directly from VDDS, you should expect an increase in current consumption with the increase in voltage. This is shown in figure 7-12…
Part Number: CC1352P Other Parts Discussed in Thread: , CC-ANTENNA-DK2 , MIOTY , UNIFLASH Tool/software: Dear Team,
Qusetion-1:
868/915 MHz: Ideal for Europe (868 MHz) and the Americas (915 MHz), with the +20 dBm PA supporting up to 5 km line-of-sight…
Hi Zack,
Thank you for the inputs.I will discuss with team and select the operating frequency.
I have 2 questions.
Qusetion-1:
868/915 MHz: Ideal for Europe (868 MHz) and the Americas (915 MHz), with the +20 dBm PA supporting up to 5 km line-of…