Other Parts Discussed in Thread: CD40106B , SN5417 I am looking for a 6 channel non inverting schmitt trigger buffer with CMOS input and output ranges. I also need at least industrial temp -40-85C, but would prefer mil temp if available. I found the CD40106B…
Part Number: CD4007UB Other Parts Discussed in Thread: CD40106B When I connect CD4007UBE as a Schmitt Trigger, the voltage on pins 2,11,13 (Vy) does not behave as expected. These pins seem to have a capacitive coupling to ground. So Vy approaches zero…
Hi Clemens,
thank you for the info on CD4000 family.
1) one question regarding CD4027B and CD4016B, how many current can they provide ? or do i need a buffer after the CD4027B?
2) is it reasonable to set a buffer after the CD4016B switch because i need…
Part Number: CD4027B Other Parts Discussed in Thread: CD4050B , CD40106B Dear *,
I attached my schematic with CD4027B. I have connected toggle button on P2 and when press the button the 14V comes to K1, J1 and through R10 10Ohm C8 100n to CLK1 but the…
Part Number: CD4050B Other Parts Discussed in Thread: UCC27527 , CD40106B
Hi
I had asked a Q reg UCC27527 Input characteristics .
This is a related Q
We want to create a Short Pulse Suppression Ckt for our 0-15 V Signals from the DSP
Typical value would…
Other Parts Discussed in Thread: CD4070B , TLE2022 , LM158 , LM193 , CD40106B , SN54LS14 , CD4012B , CD4518B , CD4052B , CD4053B , TL074 , SN54LS161A , TLC271 , LP2951 , LM117 Hello,
In order to process a database of obsolescence, Safran Electronics and Defense wishes…
Hi Pratik,
Pin 11 of the D-flip flop should be connected to the output of the VCO (pin 4 of the CD4046B).
The D-flip flop is a CD4013B, and the logic can be created with a CD4002B (4-input NOR gate) and a CD40106B (hex inverter).
I'm not sure why the…
Hey Mark,
It sounds like you understand the requirements for using dual supplies well. We can't guarantee meeting any particular specs beyond the recommended operating range, but if you stay within the abs max ratings, you should be fine. Just be…
Part Number: CD4013B Other Parts Discussed in Thread: CD40106B Hello E2E Logic Forum Members,
I have a question. Does CD4013B have an input hysteresis characteristics ?
If it is yes, would you please let me know the voltage width ?
Of course, I understand…
Hi Marshall,
May I ask why you are doing logic at such high voltages? It's rather uncommon to see.
Also, are you really leaving all the inputs to the unused OR gates floating, or is that just a mistake in the schematic? Those need to be terminated…