The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: CD4097B In the CD4097B datasheet (and in the J (R-GDIP-T**) mechanical drawing), there are Narrow and Wide dimensions given for the J package. The "C" dimension is different between the Narrow and Wide package. Does the CD4097B package…
Part Number: CD4097B Other Parts Discussed in Thread: MUX507
Dear Sir, please answer
I'd like to use CD4097B as (8:1)x2 analog multiplexer.
I have dual +/- 5 V power supply (+5V, -5V, GND).
I need to tranfer 15 mV.....3V, 50 Hz differential signal…
Part Number: CD4097B Other Parts Discussed in Thread: TMUX1108 , MUX36S08 Hello,
Can somebody please clarify whether the CD4097/67 work for low amplitude signals input at the S0-S7 terminals? (Say the order of a 50mV)?
The input voltage spec in the datasheet…
Hi Kameron, thanks for your reply. Can you kindly recommend me an alternative P/N that can support I2C and other two-line digital protocols (3.3V logic)? Do you think I should use an analog multiplexer (eg. CD4097B)? BR, Roberto
Part Number: CD4097B Hi Team,
My customer is using CD4097B and supply voltage is 3.3V(VSS is connected to GND). The control level is described at 5V and what is the input logic level when supplied voltage is 3.3V?
Thanks a lot.
Vincent Chen
Other Parts Discussed in Thread: CD4097B , TS3USB3000 , TS3DS10224 , SN74CB3Q3251 Hi,
I'm trying to use the CD4097B(PWR) as a 1:8 USB 2.0 multiplexer. Even though it's a differential multiplexer, it doesn't seem to work. Is it even possible with this chip…
Other Parts Discussed in Thread: CD4097B I am interested in demultiplexing an I2C bus and I have identified the CD4097B IC as a suitable device for the application.
My questions are as follows:
- Can CD4097B handle bidirectional data transfer through its…
Part Number: MUX507 Other Parts Discussed in Thread: SN65C1168E , , CD4097B , TMUX1308 , SN74HC151 , CD74HC238 Hi all,
My customer want to design an 8 RS485 mux with MX507 + SN65C1168E. Is it ok for using MUX507? or other suggestion for the application?
…