Part Number: DAC81408EVM Other Parts Discussed in Thread: DAC81408 Tool/software: Hi,
I have got a DAC81408EVM, and I try to control it by the SPI from my Arduino.
Here's my setting
VCC = 10V
VSS = 0V
VDD/VAA and VIO is 5V (J10 selection = VIO)
1.…
Part Number: AM2634 Other Parts Discussed in Thread: DAC81408EVM Tool/software: Hi Team,
I am trying to interface DAC81408EVM with AM2634. Below tasks are done.
SPI comm from AM2634 to DAC is established
Checked few testcases by setting output voltage…
Part Number: DAC81408EVM Tool/software: I am having an issue with DAC81408EVM when trying to transmit more than 4 channels to DAC. If I only transmit 4 channels, everything is fine. If I try to transmit more than 4 channels, then the DAC will output…
Part Number: DAC81408EVM Hello,
I hope this message finds you well. I just want to know that can I connect "DAC81408EVM" board to a microprocessor through Serial/SPI and control it. I do not want to use the software tool in PC.
In advance thank…
Part Number: DAC81408EVM Other Parts Discussed in Thread: DAC61408 , DAC81408 , REF5025 , DAC81416 Hello,
We have purchased DAC61408 Eval board, we need to generate negative output from all 8 channels. we have tried connecting Vss to negative 12V.
still…
Part Number: DAC81408EVM Other Parts Discussed in Thread: USB2ANY , DAC71408 , PSPICE-FOR-TI , DAC81408 , DAC80508 , OPA593 , DAC82002 Dear Team,
My customer is considering to use the DAC71408 (14-bit), and has the DAC81408EVM and the USB2ANY now. They want…
Part Number: DAC81408EVM Other Parts Discussed in Thread: USB2ANY , REF5025 , DAC81408
Hello Team
I'm trying to control the DAV81408EVM with USB2ANY interface adapter and GUI from DAC81408EVM software downloaded for the TI website.
I use internal 2…
Part Number: DAC81408EVM Other Parts Discussed in Thread: DAC81408 , USB2ANY Hi Experts,
Our customer dac81408 device. However he has no usb2any connector. He is asking if he can use rs232/442/485 as a usb2any device dac810408 EVM?
As far as I know this…
Part Number: DAC81408EVM
I have been using this DAC-EVM for some time, and all the ports were working fine. Recently I see that THREE out of EIGHT channels are not working.
Channels 02, 06 and 07 are giving voltages -10V, -10V and 10V respectively. My…
Part Number: DAC81408EVM Other Parts Discussed in Thread: DAC81408 Hi,
We would like to use the DAC81408 for developing the battery testing equipment and was using the EVM to do the verification.
However, we faced some short circuit issue. Just wondering…