Part Number: MCU-PLUS-SDK-AM263PX Tool/software: I´ve tried to use the AM263PX-PWR-EST-CALC tool, but it doesn´t give any results at the result fields C37, D38 ...
I think the excel file is not working.
See link below:
AM263PX-PWR-EST-CALC Calculation…
Part Number: TPS54160A Other Parts Discussed in Thread: TPS54160 ,
Tool/software:
Hi, I'm using the TPS54160ADRCR as an inverting pwr supply, from +24V to -6V following the SWIFTINV-CALC-REVE.xls excel sheet and the SLVA317B document instructions…
Hello,
The AM263P Power Estimator tool and App note explaining its usage can be found here: AM263PX-PWR-EST-CALC Calculation tool | TI.com
Regards,
Sahana
Part Number: DRV8262 Tool/software: Hello,
We used the DRV8262 in our design to power TEC elements. We connected two 12V TECs in series to a full bridge so we could use the full 24V supply voltage. In this configuration, we achieved a maximum current…
Other Parts Discussed in Thread: OPA355 Hello this is seongmun kim nowaday, i am running to simulation about noise analysis. but example noise information in macro is not correct for analysis. can i share the inforamtion about noise component for OPA355…
Hello Pablo,
Thank you for very detailed reply.
As per 8.2.1.2 I've found following details about our hardware. As per the datasheet 40khz was used. but in my case 8.96khz is used.
VM (v) (12V ~ 24V)
18
(Nominal)
Fpwm hz
8960 …
Sunil,
I'm not an expert on Orcad simulator but contrary to your error messages all of the subcircuits are defined - see below:
ERROR(ORPSIM-15108): Subcircuit VCVS_LIMIT_0 used by X_U1.XU17 is undefined
*VOLTAGE CONTROLLED SOURCE WITH LIMITS .SUBCKT…
Morning Mike, I'm using the RGT model (see below)
***************************************************************************** ** This model is designed as an aid for customers of Texas Instruments. ** TI and its licensors and suppliers make no warranties…
Part Number: LM5069 Other Parts Discussed in Thread: CSD19536KTT Hi,
We are using LM5069 on one of our power module.
The may reason for the usage of the LM5069 is to get the Supply enable/disable control, Output short circuit protection and also…