Part Number: DCH010505S Hi team,
My customer is using the DCH010505S now. We want to check whether we have short pin package below, for example, 3.15mm. Thanks.
这个型号还有没有短针脚的。目前针脚有点长。有没有 3.15mm 的长度。
Part Number: DCH010505S Hi team,
My customer is going to ues DCH010505SN7 in their design, and they're wonder what's the output voltage accuracy of this DCH010505SN7?
Please let me know if you have any ideas, thanks!
James
Part Number: DCR010505 Other Parts Discussed in Thread: DCH010505S , Hi team,
My customer is wondering why DCR010505 is more expensive than DCH010505S?
Could you please help to address some key specs or comparison table?
Thanks!
Part Number: EK-TM4C1294XL Other Parts Discussed in Thread: DCH010505S , We need the 3D models to add in our Philips library. the models in any universal format like step file.
DDR TERMINATION MODUL 15A 5V
Switched Supply Unit
PTH05010YAZ
MOD DC-DC…
Part Number: DCH010505S I have a DCH010505S which is supposed to be a 5v to 5v isolated converter. If I put 5v into it it gives 7.6v output. Whatever the input voltage the output is always about 2.5v above. What is happening? I have two of these and they…
Part Number: DCH010505S Hi,
Does DCH01X series or DCP02X series support Hot Swap? or Can we have other isolated power module support hot swap?
Thanks,
Walsh
Part Number: DCH010505S Hello,
I am assessing the feasibility of using the USB Power Delivery Specification for a portable medical device application. The intent is to provide convenient charging through USB-C, using the 9V/3A specification. In this use…
Other Parts Discussed in Thread: DCH010505S Dear support member, My Customer is considering DCH010505S.
DCH010505S, is there Isolation Voltage 2000VAC rated 1minute?
No case, Is there anything else?
Best regard. Bob Lee.
Other Parts Discussed in Thread: DCH010505S when I use the DCH010505S,I have encountered some problems that when the input voltage is 5V,the output voltage is 7.6~8V. But according to the chip manual, the output voltage should be 5V.Can you help me?Thank…