Hi Nikshith,
Please use the below attached files - 8865.txt 2364.txt Rename the above RAW video files from .txt to .yuv (e.g 8865.txt to 1.yuv & 2364.txt to 2.yuv) Create the input raw file combination of black and actual raw video -
cat 1.yuv 2.yuv…
Hi,
We are using the SK-AM62 E3 revision. Can you please confirm which revision are you testing the HDMI audio?
Shorted the j24 pins. Still HDMI audio is not coming.
Attached the boot logs for you.
Fullscreen
5367.Bootlog.txt
Download…
Could you please try the following:
1. Download the file attached. Change the extension from .txt to .bin
2. Run it from the command line with the following parameters:
"ti_simpack_vayu_ccs_0.6.2.0_setup.bin" --mode silent --prefix "/home/vasanthaangappan…
Hi,
Attached is the RAW image downloaded using DCC with these parameters:
I attached the RAW image and also the VLC image that corresponds to it. The RAW file was renamed to txt since the tool did not allow uploading of a file with extension RAW…
Hi,
It may not need to run in FDU mode. You can add MSPM0_BSL_GUI.exe in SDK installation folder\tools\bsl\BSL_GUI_EXE. Modify the attach file name from .txt to .exe
MSPM0_BSL_GUI.txt
Then run the .exe file. In MoreOption->Update XDS110 firmware…
Hello Hideaki,
I'm not too familiar with these labs, but I do have a couple of BIOS examples for F28377D that use controlSUITE. These examples use IPC to send messages between CPU1 and CPU2, though, which may be more than what you are trying to do.…
Hi Patrick,
nothing is wrong, we found out an unexpected bug in the software. The correct version will be updated by today on the website. In the mean time I can share with you this version in advance. Could you please try it out and check if you face…