Part Number: MCF8329A Other Parts Discussed in Thread: MCF8329RRYEVM Hello,
I tunned the bldc motor from GUI and saved the tunned parameters as .json formate.
I want to run the motor using GUI and/or individually (without GUI) using EVM board MCF8329RRYEVM…
Dear Alicia,
I was meanwhile successful to run a similar board LDC1101click from MIKROE via an Arduino controller. So I intend to break up the EVM and proceed that way using my own sensing coils now.
I was chosing LDC1101 for its high sample rate…
Part Number: DEM-OPA-WSON8-EVM Other Parts Discussed in Thread: OPA855DSGEVM Hi
Please can you provide the CE/EU Declaration of Conformity for DEM-OPA-WSON8-EVM ?
The product shows it bears the CE mark however the declaration is not available on the…
Part Number: USB-PD-CHG-EVM-01 Other Parts Discussed in Thread: BQ25798 , TPS25751EVM Hi team,
I’m evaluating the USB-PD-CHG-EVM-01 and would like to confirm Source operation, specifically sourcing a 20 V PDO on VBUS.
Is it supported/safe to inject…
Part Number: AWR6843ISK Other Parts Discussed in Thread: AWR1843BOOST , AWR1843 , AWR6843 , IWR6843 , MATHLIB , SYSBIOS hi sir/madam,
I want to run and visulaise the output of automated_parking application available part of "C:\ti\radar_toolbox_2_30_00_12…
Part Number: DRA821U Hi Experts,
A customer Installed Arago linux and would want to run test apps on remote cores. However, they cant run any example inside ti-processor-sdk-rtos-j7200-evm-11_01_00_02 on R5F cores. They make and build examples and get…
Part Number: AWR6843ISK dear sir/madam,
I want to run and visulaise the output of obstacle_detection_aop application available part of "C:\ti\radar_toolbox_2_30_00_12\source\ti\examples\Automotive_HandsFree_Access\Door_Obstacle_Detection\obstacle_detection_aop…
Part Number: AM261-SOM-EVM Other Parts Discussed in Thread: SYSCONFIG Hello!
I am trying to run the Profinet device example from TI industrial communications SDK (I tried both versions 10.02.00.17 and 2025.00, the same behavior was observed) on my AM261x…
Part Number: F29H85X-SOM-EVM While trying to load the RAM-based HSM runtime (KP/CP provisioning HSM RT) using the RAM-based UART SBL, the SBL responds with a NAK after receiving the .HSMIMAGE. How can this issue be resolved?
Regards,
Shashank