Part Number: AM5708 Other Parts Discussed in Thread: AM5728 Hi:
I have a custom AM5708 based board with SDK6.02 Linux RT.
The board has 3 ethernet interfaces:
- eth0: connected to GMAC
- eth1: connected to prueth pruss2_eth
- eth2: connected…
Hi Paula,
Thank you for your help. We tried to run the encoder several times yesterday. This is the main function.
void main(void)
{
printf("IPC start\n");
Task_Params taskParams;
/* Call Ipc_start() */
printf("IPC finish\n");
Ipc_start…
Anders,
I will look into this. The data sheet is currently being revised to included a power up sequence (see attached). Are you following this sequence?
Regards,
Jim
7450.SBAS756B_Draft3_01192017.pdf
Dear George,
I compare the two map files, but I can not determine what functions or data are related to the error. would you help provide us with some relevant file?
The two map files are shown in the attachment. Thanks.
5265.Project.txt Project_Lib…
hi,DavidL
(1)i have done what you said in order, after the 3th step according to your advice,and i read the msp432 via MSP-GANG,
read_from_msp432.txt
(2) after that i failed to conect to bsl using msp-fet too!
so i am superised that :
if i don…
Hi Nikolai,
ads52J90_Data_Sheet(10_22_2018).pdf
How are you?
The input signal connections INPx and INMx for ADS52J90 is not the same as ADS5295's.
When you are using ADS52J90 device,
please refer to its Datasheet page 70 (for AC coupling…
Hi Dhanasekaran,
Sorry for the delayed response. Please refer to the register map of the TLK10232 that is the same of TLK10031, in this document you will find all reserved registers to understand in a better way the bring up procedures. Even the TLK10031…
Anders,
The device does not support PRBS and this will be removed from section 8.4.2.2. We are currently revising the data sheet. See the attached copy. For the answer to question #2, the JESD_MODE needs to be set to 0x04 for LMF = 421.
Regards, …