the issue is that i do not have the TI EVM hardware to test my module on, i use my TRF with a Psoc MCU for this project (so i can not do it this way). i've already read the REV.B project and i can confirm that they have mentioned only the ISO CONFIG …
Adding more debugging output resolved the arm_reserve_mmu issue.
I added a #define DEBUG at the beginning of following files:
arch/arm/lib/cache.c
arch/arm/cpu/armv8/cache_v8.c
arch/arm/mach-k3/j721s2_init.c
board/ti/j721s2/evm.c
common…
I used the HW BOM file tool to compare the BOM with Digikey and Greensoft, and all of the components are REACH compliant. I then submit a request to PRSC team to ask them to create the EU Declaration of Conformity based off of this BOM compliance data…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: LAUNCHXL-F280039C , DRV8353 Hi Team
the DRV8353RS-EVM mention it's
"FOR USE ONLY WITH TI ISO-F28027F”
so this board can be only used for ISO-F28027F? or it can work with LAUNCHXL-F280039C…
Hi,
Your configuration looks correct and based on your data captures, it appears that the TLK receiver is achieving alignment correctly. Your data captures indicate that the receiver sporadically sees errors, and the RXD values mirror this.
What are…
Hi Varun-san,
Thank you for your waiting.
I checked the voltage of your mentioned as below.
TP13 : 3.27V
TP14: : 3.27V
TP15 : 1.773V
TP17 : 1.773V
TP10 : 3.411V
TP5: 5.125V
And about J11 and J12, both jumper settings are "open".
I…
If only one IQ is provided from the iso gate driver data sheet, then use that value for IQ_DRIVER_VDD and IQ_DRIVER_VEE in the Excel tool. Also recommend to use RLIM configured as RDR as described in the Excel tool. Draw the schematic similar to what…
Part Number: LMK5C33414A Other Parts Discussed in Thread: LMK5B33414 , LMK5C33414 , Tool/software:
Hi,
I have two questions relating to the LMK5C33414A:
1] I am trying to simulate the phase noise profiles at the output of an LMK5C33414A using PLLatinumSim…
Hi Aaditya Vittal; We removed U3 and lowered the pull up resistors R5 and R6 to 1K. We tested it like this and it didn't work. This test was done with two ISO1641BDRs as per the diagram below. µC ---- ISO1641BDR========cable=de=1MT========ISO1641BDR …
Part Number: AM68A Tool/software: Hello,
We have a custom board using an AM68A. I am in the middle of evaluating USB Boot mode and I'm running into some issues. I can properly set the device to usb boot mode and my computer enumerates the device as…