Hi Downey,
The PCM9211 works well and would have the flexibility of adding analog to S/PDIF and many other conversion options for future designs.
A simpler solution would use the DIT4096 and DIT4192 devices which are specifically meant for Audio Serial…
Part Number: PCM9211EVM-U Other Parts Discussed in Thread: PCM9211 , DIT4096 , DIT4192 Tool/software: Code Composer Studio Can PCM9211 support converting I2S to S / PDIF?
How to set up the register and GUI, do I need MCLK input?
Part Number: DIR9001 Other Parts Discussed in Thread: DIT4096 I am interested in encoding 8 on/off signals and sending them over DIT4096 / DIR9001 using the user bit. Could you give me some ideas for hardware chips and connections to multiplex them and…
Hello,
Regarding device
PCM1863 or DIT4096
In Software mode, a serial control port is used to write and read on-chip control registers and status buffers.
If I use the TI MSP430 LAUNCHPAD, what is the I2C framework for the I2C serial control port communication…
Other Parts Discussed in Thread: OPA355 , OPA343 , LM2611 , DIT4096
OPA355NA
OPA355NA/3K
OPA355NA/250
DIT4096IPWR
OPA343NA
OPA343NA/3K
OPA343NA/250
Hi,
I need ESD information for mentioned parts. Kindly provide us data.
1)Human Body Model…
Part Number: TM4C123GH6PZ Other Parts Discussed in Thread: DIT4096 , PCM3060 Tool/software: Starterware Hi people,
I implemented the software example SPMA042b on my Tiva C and I can play files from my SD card so far but the ouput sound is scratchy... it…
Hi Pedro,
You could consider an application using an ADC and then a digital interface transmitter; this could be something like PCM1864 as ADC and DIT4096 to interface into optical fiber.
Or you could also consider a transceiver solution like PCM9211…
Other Parts Discussed in Thread: DIT4192 , DIT4096 , SRC4192 Hello,
When the SRC has no input at all fed to it, does it still produce i2s outputs?
Thanks!
Hi Charlie,
An I2S to USB interface can be a combination of USB codec like PCM2902C with S/PDIF input and DIT4096 which converts I2S to the S/PDIF.
Another option is to use TMS320C5533 which is the replacement part for TAS1020B.
Best regards,
Ivan…
Other Parts Discussed in Thread: TLV320ADC3101 , DIT4192 , DIT4096 Hey all,
Doing a portable application here. It seems like I can but can someone confirm that I can use TLV320ADC3101 as an I2S input to S/PDIF output converter with I2C control?
Regards, …