Part Number: DM385-AR0331 Question, Is it possible to get raw image data before ISP processing start ?
14bit raw image camera sensor connected to EVB of DM38X chipset and I saw the document on below link that there is VIP and VPDMA handle image data. …
Part Number: DM385-AR0331 In the camera initialization code, linux_prcm_ipcam.c, there is a routine, SGX_Disable, which sets registers 0x48180900, 0x48180F00, and 0x48180F10, but these registers are not documented in the datasheet and the naming convention…
Part Number: DM385-AR0331
I'm happy to report that the rings observed are HW related. (Since I'm on the FW/SW team, we tend to blame HW for observed problems...)
A second proprietary set of boards with the same exact FW does NOT show the rings…
Part Number: DM385-AR0331 The IPNC RDK v. 3.8.1 comes with an installer for your Image tuning tool v.3.0, but the application has as a prerequisite v7.13 of the Matlab Runtime libraries from Matlab R2010a, v7.10. This is no longer available online and…
Hi Mechi,
Did you confirm whether the truncation is causing the problem or not ?
In HDR mode it is not must that sensor ALTM has to be enabled. We can use companding and do tone mapping in DM385 side using WDR module. This is how TI has integrated AR0331…
There are 2 contexts in the AR0331 sensor registers. Each context can be set according to the resolution you want. For the snapshot, change the context, capture a full frame and then go back to context A. See data sheet page 42 - Real-Time Context S…
Other Parts Discussed in Thread: DM388 , DM385 HI TI experts,
Can someone give me detail on IP camera model name which are present in the market, made based on dm388/dm385 SOC and AR0331 image sensor?
Other Parts Discussed in Thread: DM388 Hello,
I want to use APTINA AR0331 sensor builtin ALTM functinality in HDR mode with DM388 IPNC_RDK_3.8.0.
As per the given details in sensor developer guide, Sensor registers are configured. The output image is very…
Other Parts Discussed in Thread: DM385 Hi, experts.
I have dm385 IPNC - AR0331 aptina sensor.
As I know AR0331 sensor has a WDR feature.
but dm385 IPNC - AR0031 doesn't have a this feature.
When are the dm385 IPNC planning to support this feature? …