Part Number: DM388 Hi All,
We are using IPNC_RDK_3.9.1 SDK and my aim is to is input RGB24bit(full rage 0-255) and output RGB24bit( full rage 0-255) . The goal is achieved bit input RGB and Output RGB color is not matching.
Following are detailed info…
Part Number: DM388 Tool/software: TI C/C++ Compiler Hi all,
I am using IPNC_3.9.1 rdk. I am facing some problem to build.
# Making syslink-rtos in ti/syslink /home/build/VIO-Debug-hardik/Source/ipnc_rdk/../ti_tools/xdctools_3_25_05_94/xdc XDCBUILDCFG…
Part Number: DM388 Other Parts Discussed in Thread: AM5728 , AM5718 , AM5729 , AM5708 , AM5749 Tool/software: Code Composer Studio DM388 is having two video input port and one video output port is also there. Can I have PIP feature at the output video, in…
Part Number: DM388 Hi,
I am using DM38X CSK.
I am not getting how to set the values of HS_SETTLE and HS_TERM of the register "ISS_CSI2_PHY_REGISTER0" .
How to calculate this HS_SETTLE and HS_TERM timing parameters.
Senor connected is OV5640…
Part Number: DM388 Hi sirs,
We have implemented UVC driver on DM388 to support UVC camera.
However, we found that, the UVC camera sometimes fails to initialize
when user plugs in USB connector with PC.
In normal case, once user plugs in USB cable to…
Part Number: DM388 I'm trying to get started with the camera evaluation kit. For starters, the SD card shipped with the kit was loaded with apparently wrong s/w, and the device would not boot at all, only showing "CCCCCC" on the debug port.…
Part Number: DM388 Tool/software: TI C/C++ Compiler Hi all
I am using DM388 and can enable separate 16bits cameralink (CAM IF) or 16bits capturelink (VIN Port [0]).
But when I merge them together for work concurrently, only capture link can work, the…
Other Parts Discussed in Thread: DM388 Tool/software: TI C/C++ Compiler
Hi ti engineer:
We used Appro_avi_save to store avi video,now wo want to playback it on dm388, Please give guidance ,thinks.
Part Number: DM388 We use DM388. Software is IPNC_RDK_V3.8.0.
Device can output HDMI 1080p correctly. But eye diagram is not good, it can not pass HDMI certification.
I found a post.
https://e2e.ti.com/support/processors/f/791/t/431175
There is a 0x46c00310…