Part Number: DP83849IFVS-EVK I used TI's demo interface board designed for DP83849.
And use the jumper to communicate with the demo board using the FPGA, and use the photoelectric conversion head (ALLRAY-a Chinese company) ATR-01105CMT/D-ST
The current…
Part Number: DP83849IFVS-EVK Hello, i want to communicate with both rj45 ports to the fiber at the same time. I mean i will use port A and port B (rj45) simultaneously (They will share time of course) and i will communicate through fiber at the same time…
Part Number: DP83849IFVS-EVK
Hi team,
The customer is using DP83849IFVS-EVK. The A port can output the data. The led_speed of the A port is turned on all the time.
But he cannot output the data for the B port. When he enable FX-EN,AN0,AN1 and ANEN_B using…
Part Number: DP83849IFVS-EVK I can’t communicate with my device through mdio with usb to mdio tool using msp430g . Device is not giving mdc. Only a stable high on the mdc pin. Plz help
Part Number: DP83849IFVS-EVK
First of all, I'm a Chinese, but the Chinese reply is too slow. I'm a little anxious, so I'm asking questions here. 1. I only want to use the PORT B fiber output now. I don't need Fiber to copper Media Conversion…
Other Parts Discussed in Thread: TIDA-00306 , DP83849IFVS-EVK Hi all,
What is the difference between DP83849IFVS-EVK and TIDA-00306 Media Converter Board? AVAGO AFBR-5803Z is included?
Regards, Toshi
Other Parts Discussed in Thread: DP83849IFVS-EVK I have purchased two of your DP83849IFVS-EVK/NOPB Ethernet Transceiver evaluation kits. I want to use their fiber optic transceivers so that I can connect the two boards using fiber optic (fly by light)…
Hi Yash,
The termination scheme for the fiber optic transceiver is generally mentioned in the transceiver datasheet. If you look at the DP83849IFVS-EVK, the transceiver used there is the HFBR-5803. In the datasheet for HFBR-5803, there are termination…
Talents,
Here is the schematic review feedback:
I have the following comments for the schematic review:
MDIO: pull-up is recommended to be 1.5k
MDC: Remove pull-up, no pull- needed for this pin
Strap resistors: Use 2.2k (1% tolerance)
Power supply…
Part Number: DP83849I Hello,
Our customer use the DP83849 demo board( www.ti.com.cn/.../DP83849IFVS-EVK) to communication with FPGA. He used
ATR-01105CMT/D-ST for optical to electronics conversion.
The test result is as following:
The optical interface…