Part Number: DP83TC814S-Q1 Hi,
We are using DP83TC814S in our application.
External 25 MHz crystal is connected on XI and X0 pins.
Is it possible to generate this 25 MHz on CLK_OUT pin? If yes, can anyone share the procedure?
Thanks for your time.
Regards…
Part Number: DP83TC814S-Q1
I see the lots of link status indication in datasheet , what the different between them? or which one I should use better to get the link status?
1:Register 0x0001,bit 2
2:Register 0x0010,bit 0 (duplicate register 0x0001,mentioned…
Part Number: DP83TC814S-Q1 Other Parts Discussed in Thread: DP83TG720S-Q1 Hi,
I'd like to understand how can I test DP83TC814S-Q1 (or similar family part) SGMII signals on my pcb. I want to make sure that the I/Q LVDS signals are toggling properly on…
Part Number: DP83TC814S-Q1 Can you tell me why the optimized register values are not used as the default values? It was mentioned in another post, but the answer wasn't shared.
Part Number: DP83TC814S-Q1 Hi Team,
Hope you are well!
Reading through SNLA389A, Table 3-2 Mode Configuration the optimized parameters will "enable shorter linkup time" in the DP83TC814 part.
How do these optimized parameters work and when should…
Part Number: DP83TC814S-Q1 Other Parts Discussed in Thread: USB-2-MDIO I'm using the USB-2-MDIO application to investigate link behavior of a DP83TC81S-Q1. When I connect to my board, I see PHY0 through PHY15 listed as available. The behavior I was…
Part Number: DP83TC814S-Q1
Hi Expert!
We are using DP83TC814S-Q1 in our custom HW.
Current we are facing - PHY is not found on the MDIO bus issue.
qcom,emac: MDIO device at address 0 is missing
.
We have checked the DP83TC812 Troubleshooting Guide
…
Part Number: DP83TG720S-Q1 Other Parts Discussed in Thread: DP83TC814S-Q1 Hi Team,
Hope you are doing well!
1. Can you provide the configuration file of DP83TG720S-Q1 Ethernet PHY? 2. Can DP83TG720S/R/-TC share a PHY configuration file?
Thanks!
Part Number: DP83TG720S-Q1
Attached are the latest drivers tested on Kernel 5.10: GitHub - TexasInstruments/ti-ethernet-software: Repository for Ethernet PHY drivers for Linux and RTOS.
The DP83TC812 driver can be used for the DP83TC813 and DP83TC814…