Part Number: DPHY440SSRHREVM Hi,
We are planning to use DPHY440SS device for my custome design. I need DPHY440SSRHREVM board file for reference. Please do the needful
Thanks,
Sankar.K
Part Number: DPHY440SSRHREVM Tool/software: I am testing DPHY440SS EV Kit to check whether it works well in my intended design.
But the EV kit doesn't work well when testing it.
I want to show you this status, but image file uploading is locked in…
Part Number: DPHY440SSRHREVM Hello Guys,
Good day.
Our customer is looking for the mechanical dimensions of the DPHY440SSRHREVM including the support holes dimensions.
Thanks and regards,
Art
Part Number: DPHY440SSRHREVM Based on TI, DPHY440 supports up to 5dB at 750MHz and 2.5dB DE on its TX. Can I understand that retimer RX can compensate 5dB channel loss and retimer TX can compensate 2.5dB channel loss (processor EQ not included)?
Thanks…
Part Number: DPHY440SSRHREVM Some important mechanical dimensions of this evaluation board are missing. The J1 side of the board is ~2mm offset from the J2 side. The only relevant measurement given is the distance from one end of the board to J2. The…
Part Number: DPHY440SSRHREVM I tried interfacing my camera with DPHY440SSRHREVM, the input signal is 1.8V and the output signal i get is around 2.2 volts.
But I need MIPI signal in 1.8V only.
Is there anyway to configure it for 1.8V ?
Part Number: SN65DPHY440SS Other Parts Discussed in Thread: DPHY440SSRHREVM Hello,
I'm running into a problem with this part. First, a little back story. I've already verified the part works in my system using the eval board. Now I've brought the…
David,
thanks.
Is channel response simulation the software below?
SN65DPHY440SS S-Parameter Model.
Besides,
is it possible that you send me the PCB file of DPHY440SSRHREVM?
Hi, Jonard
Correct, eval board will give them a good approximation through direct measurement. There is a DPHY440 eval board available on ti.com, https://www.ti.com/tool/DPHY440SSRHREVM .
If they can measure the loss of the 30cm and 50cm at the Nyquist…