Part Number: DRA726 Dear Mr/Mrs,
We are working on a custom DRA726 board. It has been working for several weeks without any issue (booting highest priority SD, second eMMC). After making an external HW W/A (not related with DRA) it has stopped boot.
…
Part Number: DRA726 We need to do conversion from NV12 to RGBA8888 to display a camera? When done with videoconvert it is extremmely slow.
RGB is the only video format that embedded wizard support. Deinterlace is done with VPE and we end up with a NV12…
Part Number: DRA726 Other Parts Discussed in Thread: TDA2 , I am working on getting our cameras supported in IPU1 and have a question on Virtual DRM
I have been reading "Virtual DRM : An User Guide for Developing Usecases". It seems straightforward but…
RamPrasad,
As I look to implement the usecase I see that I cannot use iss_capture since the Image Subsytem doesn't exists in the DRA726.
As I look thru the technical manuals of the DRA76 and DRA726 I see that their CSI2 ports are similar except that…
Part Number: DRA726 I see this on multiple wikis,
"NOTICE: The Processors Wiki will End-of-Life in December of 2020"
Is there going to be an alternative, if so what?
Since I can't get the EGL to work with kernel 4.19 I am going to plan B for…
Part Number: DRA726 Other Parts Discussed in Thread: TDA2HV , , AM5716 , AM5728 , AM5708 , AM5726 , AM5746 , AM5718 , AM5748 , AM5749 , AM5706 , SYSBIOS , TDA2E Could somebody advice what to do with next errors:
**** Build of configuration Debug for project k2h_to_dra72x_arm15…
Part Number: DRA726 We use pulseaudio to play USB music,then there's a 100% probability of a broken tone, the kernel alway print follow logs:
[ 54.788437] davinci-mcasp 48464000.mcasp: Transmit buffer underflow [ 54.788726] davinci-mcasp 48464000.mcasp…
Part Number: DRA726 If fixed the command line issue with kernel 4.19 but can't get weston to work.
[13:24:55.431] weston 5.0.0 wayland.freedesktop.org Bug reports to: gitlab.freedesktop.org/.../ Build: unknown (not built from git or tarball) [13:24…
Part Number: DRA726 I am working on TI-RTOS support for our analog cameras.
The I2C port used is I2C6.
There are some definitions missing since TI official code doesn't support it.
We've had no issue so far on Linux since we do not use uart7 …