Francois,
Is the customer using the recommended TPS65903x as the power solution? If so:
"If the RTC-only (sleep) mode is supported by the design, check that VDDA_RTC, VDD_RTC and VDDSHV5 are powered by separate supplies and are not combined with other…
Part Number: DRA750 Hello Support team,
Kindly I need to know the minimum density per die, Maximum Density per die, Total Density per Die for DRAM for this part Number DRA750.
Appreciate your fast reponse.
Part Number: DRA750 Hi Expert, This is to confirm DRA750 I2C3 behavior (and it is related to DRA750: I2C3 behavior & How to recover from I2C issue ) Customer is using FAST mode on I2C3.
According to DRA75x DataManual Table 7-36 above, th(SDAL-SCLL)…
Part Number: DRA750 Hi Expert, My customer wants to confirm regarding Jacinto6 I2C3 behavior and asks us to propose how to avoid issues with Jacinto6. ----- 1.Background This questions is not a problem happened in Jacinto-6, but it happens with Competitor…
Part Number: DRA750
The customer works with Ubuntu 16.04 machine while the processor SDK Linux Automotive is recommended to build with Ubuntu 14.04. or Ubuntu 16.04 (see link below).
https://processors.wiki.ti.com/index.php/Processor_SDK_Linux_Autom…
Part Number: DRA750 Tool/software: Linux Hi,
I am following below steps but I get errors:
1. follow section 2.4; make linux; make linux_install (still I don't get EGL under targetfs)
2. Select make config in Rules.make
TDA2XX
MAKECONFIG=tda2xx_ev…
Part Number: DRA750 Other Parts Discussed in Thread: SYSBIOS
Tool/software: Code Composer Studio
if i config .cfg like the attachment , the cpu load graph is empty when checking using ccs and XDS560v2STM debugger .
rtos and uia installed
xdctools_3…
Part Number: DRA750 Hi Suhas,
I am working on a board based on TI J6 dra76x and have the same error than you posted here.
[ 4.277569] remoteproc0: failed to load dra7-ipu1-fw.xem4 [ 4.277582] remoteproc3: failed to load dra7-dsp2-fw.xe66 [ 4.277622] remoteproc2…
Hi
Dont have additional inputs nor immediate plans to enable FIQ handling support - though we will follow-up closely with any updates in the mainline kernel for such support.
Will mark this as closed for now