Part Number: DS110DF410 Other Parts Discussed in Thread: DS250DF410 , , DS250DF810 , DS280DF810 Does the DS110DF410 and DS250DF410 support these features?
1、Does TI's retimer guarantee that the input Serdes signal is at the same frequency as the output Serdes…
Part Number: DS280DF810 Other Parts Discussed in Thread: DS110DF410 , , DS125DF1610 Hi Expert,
Looks like DS280DF810 and DS110DF410 are very similar, but the DS280DF810 data rate is higher.
DS280DF810 have VGA except CTLE and DFE compared with DS110DF410.
…
Part Number: DS110DF410 Hi Team,
We are using DS110DF410SQ IC in our design and we are not getting the video output as expected ( we are using it for ARINC 818 video stream)
I have attached the overall setup and how we are debugging this, and we have few…
Part Number: DS110DF410
1、During the test, when the temperature drops from 70 ℃to -20 ℃, The average time rate drop by 1℃ in 1 min ,it comes up-down around 0 ℃,what is the cause of this phenomenon,as follow:
2、How to configure the CTLE by manual operation…
Part Number: DS110DF410 Hi Expert,
The customer is adopted the DS110DF410SQ into switch applicant.
May we have your support to review customer's schematic design?
Thanks
Best regards,
Eric Lai
Field Application Engineer
Texas Instruments Taiwan…
Part Number: DS110DF410 Hi team,
May I ask why capacitive isolation is required in the above figure ?
After the resistance 100 ohms, 2.5V is divided into 1.75V, but the high Viet threshold is also specified…
Part Number: DS110DF410 Hello, My customer is designing L2 switch product. They would like to support both 1G ether and 10G ether. They are considering DS110DF410 as a candidate of a retimer. Can DS110DF410 be also used for 1G ether (1.25Gpps rate)? …
Part Number: DS110DF410 Dear Expert
I have a question about the data rate of DS110DF410, I would like to consult the original factory, thank you! The details are as follows:
1. If the data output mode is set to RAW Data, the CDR circuit is not used. …
Part Number: DS110DF410 Hi, team
my customer use DS110DF410 for ethernet data rate, and want to switch between 1.25G 2.5G and 10.3125G automatically
according to table 2, if we write 0x2f to 0x06, it could get 1.25 and 10.3125Gbps.
according to table 3…
Part Number: DS110DF410 Dear Expert
1. What is the meaning of RWSC as shown in the figure below? Is setting this bit, 0x2F[0] to 1, going into CTLE's adaptive mode? In this mode, instead of setting the EQ seting value, the device will automatically…