Part Number: DS110DF410 Dear Expert
1.configuration procedure as follow, is it right?
a. setting Rx EQ/DFE ,and click Apply to ALL Channels ...
...
b. setting CDR(assume the Manual Mode)and then click Apply to ALL Channels
My question is :
(1)PPM Tolerance…
Part Number: DS110DF410
Hi Team,
Please advise me on a question bellow.
I am using DS1100DF410 connecting to an optical module.
During the system test, DS110DF410 report poor eye opening, when I referred address 0x27 and 0x28,
resulting excessive error…
Part Number: DS110DF410
Hi team,
Could you please share some information about how to configure the 0x03, 0x3a.0x40 for the CTLE? Do we have some reference code or the register map can share? Thanks.
The left side is good configuration, the right side is b…
Part Number: DS110DF410 Dear Technical Support Team,
Q1)
According to the App Note(SNLA323),
the procedure is describe for writing 0x04 to register 0x00 and returning the register status to the default before setting the equalizer / retimer of Channel…
Part Number: DS110DF410 1. Is automatic data rate identification supported or must be configured?
2.The circuit topology we use is shown in the figure below. So we could use it in master mode or slave mode.
My question is ,are there any temporal constraints…
Part Number: DS125DF111 Other Parts Discussed in Thread: DS110DF111 , , DS100DF410 , DS110DF410 , DS125DF410 Tool/software: In this FAQ, I will cover the SMBus register sequence to capture a full eye opening measurement. This FAQ applies to the following…
Part Number: DS110DF410 Other Parts Discussed in Thread: DS125DF410 , DS250DF410 Hi,
I would like to ask you to tell me upgrade device fo DS110DF410?
My customer is looking for the device which is higher speed than DS110DF410 and the requested specifications…
Part Number: DS110DF410 Other Parts Discussed in Thread: DS125DF410 Dear colleague,
Customer want to add a retimer between 2 FPGAs, the data rate is 10.3125G, but the data format is custom.
So they want to know whether the DS110DF410 is suitable.
And…
Part Number: DS110DF410 Hi team,
We want to check whether the REFERENCE CLOCK is must. From the datasheet, it seems to be must have. But when we pull the pin to GND, the device can also work. Could you please help check it? Thanks.
Part Number: DS110DF410 Other Parts Discussed in Thread: DS125DF410 Hi,
1. Does DS110DF410 support 11.34375Gbps? The datasheet describe the data rate range is from 8.5 to 11.3 Gbps.
2. If DS110DF410 could support 11.34375Gbps, how to set the 0x2F register…