Part Number: DS110DF410 Hi Team,
Can you share DS110DF410 updater file to us? then we can use the GUI to adjust the setting.
My mail: Oliver-Ou@ti.com
Thanks.
Oliver Ou
Part Number: DS110DF410 Hi TI,
Please could I request information on details of the PRBS31 pattern generated by the intnerla PRBS Generator?
Such as information on the characteristic polynomials for the PRBS31 pattern?
Thanks,
Sean.
Part Number: DS110DF410 Hi TI,
I am using the DS110DF410EVK evaluation board with a clock input directly from a coax of 644.3125MHz. From this I am trying to generate a 10.3125GHz PRBS 31 pattern.
Presently I can see that there is an input successfully…
Part Number: DS110DF410 Hi TI,
I've been testing the DS110DF410 on my test card. This is 12 DS110DF410 transmitting 48 channels of PRBS31 data at 10.5 GHz. These channels are being output onto short tracks to an optical transciever and received by an…
Part Number: DS110DF410EVM Hi all,
I am programming the retimer device onbard the EVM through I2C with a MCU broken out from another device.
I can achieve comms with the IC successfully and performs reads and writes on the device.
For the inputs I am…
Part Number: DS110DF410 Dear Technical Support Team,
I have been debugging for CDR unlocked issue with DS110DF410.
Questions:
1.) Could you share the appropriate setting for 11.0957Gbps?
According to 8.4.4 Standards-Based Modes, the procedure is as…
Part Number: DS110DF410 Hello,
The channel register and shared register use the same address, I need to change the global register to choose which register can be changed, am I right?
But I find I set the global register to 0x05, 0x03, then it could be…
Part Number: DS110DF410 Other Parts Discussed in Thread: DS125DF410 , , DS100RT410 , DS110RT410 Hi TI Support,
I should preface that this question is part of an ongoing investigation. I have looked at several retiming products with an interest of generating…
Part Number: DS110DF410 Are there screen captures of Eye Monitor of SIgCon Architect available to view / download.
Thank you.
Andrzej Hadas
AZ-COM Inc.
925-254-5400
ahadas@az-com.com
Part Number: DS110DF410 Hi,
My question has below question for retimer DS11DF410, Can help to check and give some suggestion? Thanks a lot.
The Retimer chip has 25M refclk output. How is the clock generated inside the chip? Is it the recovered from CDR…