Part Number: DS125BR111 Hi TI team,
The repeater DS125BR111RTWR is being used in our design and it is configured in pin mode. But our device is not being detected by HOST.
Only this re driver IC is present in between host and device. Can you please confirm…
Part Number: DS125BR111 The data sheet for DS125BR111 states the maximum operating temperature (85 deg C) and maximum storage temperature (125 deg C), but those are both based on ambient temperature conditions, usually at the case. What is the maximum operating…
Part Number: DS125BR111 Hi,
I would like to know there have recommend layout distance from DS125BR111 to CPU and from DS125BR111 to 10G SFP Connector?
thanks!
Jeff
Part Number: DS125BR111 Hi there,
I want to know what's the size and shape of thermal pad for the two devices below.
1. DS125BR111RTWR
2. DS80PCI102SQ/NOPB
they are both RTW package drawing, however it is said the size and shape of the thermal pad…
Part Number: DS125BR111 Can EQA1 and EQA2 be connected directly to GND instead of pulling down to GND with a 1k resistor(shown in DS 8.3)?What is the influence on overall functionality ?
Part Number: DS125BR111 Hello team,
Could you please tell me how much current can go through VDD?
It's pretty sure to be above 60mA(Idd: max), but the customer would like to know this specification while considering the safety for their circuit. (e.g…
Part Number: DS125BR111
Hi Sir,
Q1. DS125BR111 can support SATA3 which is 3GHz, but I don't see the equalizer compensate table to mention about the EQ value on 3GHz,
Can you please help to clarify the exactly value of equalizer in 3GHz?
Q2. What…
Part Number: DS125BR111 Hi Sirs,
Sorry to bother you
Two questions on DS125BR111
1. If our signal insertion loss will be 30db, could we use serial connect for large insertion loss application
2. If we use EEPROM control, do we need one EEPRON by one solution…