Part Number: DS125DF111 Hi Team,
Can you please let me know what is the maximum junction temperature of this device? can you also share the recommended continuous operating junction temperature?
Thank you kindly,
Regards,
Marvin
Part Number: DS125DF111 Other Parts Discussed in Thread: DS250DF410 , Hi experts
We've been using the instructions in this app note ( www.ti.com/.../snla386.pdf) to estimate junction temperature on DS250DF410 retimers.
Is there a similar procedure we…
Part Number: DS125DF111 Hi Team,
May I know how to disable the DS125DF111 DFE and CTLE function? I only want to use the amplitude limitation function of this device. Thanks.
I tried to disable the DFE in GUI, but it doesn't work. And does CTLE=0 means…
Part Number: DS125DF111 I have an application which uses (2) DS125DF111, one on each sides of a coax cable, in a 10GBE application. I want to set the DFE Tap 1 manually but when I do that the system does not link after bootup unless I go into the GUI…
Part Number: DS125DF111 Hello,
We are using DS125DF111S in our custom Board for 10G SFP. LOS output is low .
Inputs to device is verified in oscilloscope. LOS output from device is low .
TX_DIS input to device is low to enable the output ports. However…
Part Number: DS125DF111 Is the DS125DF111 a MMIC? Is it Silicon Based? Is there any reason not to consider this device as a MMIC?
Monolithic microwave integrated circuit , or MMIC (sometimes pronounced "mimic"), is a type of integrated circuit (IC) device…
Part Number: DS125DF111 Hi Expert,
The DS125DF11 1 is used the WQFN package.
It defined the max height is 0.8 mm max.
The engineer is asking the tolerance of this spec.
Pls advice.
Eric
Part Number: DS125DF111 Hi Team,
Could you help please help? We have question regarding DS125DF111 a multi protocol CDR.
First: the jitter tolerance is speciified at 10G in the data sheet
what about the jitter tolerance going to halve or…
Part Number: DS125DF111 Other Parts Discussed in Thread: DS110DF111 , TI Design Support Team:
Please advise on DS125DF111 and DS110DF111 programming data rates (0x60-0x64).
We have designed and test the DS110DF111 at various data rates for our product,…
Part Number: DS125DF111
For some reason, when laying out the PCB,i need to set the input and output of DS125DF111 as shown in the figure, the input is OUT_P --- INA- \ OUT_N ----- INA+, and the output is also OUTA- ---- TD+ \OUTA+ ----- TD-, my question…