Part Number: DS250DF410 Hi Support Team,
the DS250DF410 has a clock in --> Buffer(Inverter?) --> and a clockout.
Is it possible to combine these inputs and outputs with a crystal for a pierce oscillator?
Or is it better to have a single endet XO…
Part Number: DS250DF410 Hi Team,
Customer wants to verify if this device both TX and RX differential output impedance is 100 ohms, correct?
Customer points out we only address RX differential 100 ohms but not for TX and if any special reason behind, thx…
Part Number: DS250DF410 Other Parts Discussed in Thread: USB2ANY Hi Team,
Customer wants to use internal PRBS Generator, but cannot make it work through USB2ANY.
They confirm communication is good, they can successfully read/write.
May I know the correct…
Part Number: DS250DF410 Hi
I would like to ask you some questions as below.
Though my customer has been trying to use PRBS function, they have failed to get output PN pattern signal yet.
They set the register setting by "SNLU182B 6.22".
Q1)…
Part Number: DS250DF410 Other Parts Discussed in Thread: DS125DF410 Hi,
I would like to ask you a question about the value of "Reg 0x64" from my customer as below.
1) Setting value
Let me comfirm that we can set the "lock range" of the signal…
Part Number: DS250DF410 Hi,
let me ask you a few questions:
1) For 10GbE
If we would like the tolerance to be around 100 ppm, we should set the "0x02" to Reg0x64 (=approximately 151 ppm), correct?
2) Register setting procedure
If we change the…
Part Number: DS250DF410 HI experts,
Customer have question regarding 9.2.3.1 AC coupling capacitors in the range of 100 to 220nF are required for the RX inputs and TX outputs.
1. Please kindly let them know the most recommended caps? For example, smaller…
Part Number: DS250DF410 Other Parts Discussed in Thread: DS125DF410 Hi Team,
Please advise me on my question, on how to calculate PPM tolerance of DS250SD410.
I suppose that, focusing on VCO1, the registers 0x61 and 0x60 record VCO count
value and 0x67…
Part Number: DS250DF410 Other Parts Discussed in Thread: DS280DF810 How do I write the register setting value when I want to use DS250DF410 with the configuration below?
rate : 25.78125Gbps
Part Number: DS250DF410 Hello all,
I'm developing camera sensor hardware.
developing camera sensor is too high resolution sensor (24MP) to transmit with serdes.
so I'm interested in long transmission data within mipi- csi2 protocol .
Is DS250DF410…