Part Number: DS250DF810 Hi Sir,
Could you please share the IBIS model for DS250DF810? we need to run the simulation the design with DS250DF810
Thanks
Jialin
May I ask when the input eye diagram parameters (0x27, 0x28) from the optical module to the ds250df810 can be correctly restored when the ds250df10 is in 10G mode? We have observed that the DS250DF810 on site receives signals from the optical module,…
Part Number: DS250DF810 Other Parts Discussed in Thread: TUSB1104 , SN65DP141 , TDP142 , TDP2004 , TUSB2044 Dear team,
Do we have suitable solution can replace below? Thanks a lot.
Item
Signal
RVP using model
Description
Vendor
1
USB3.2…
Part Number: DS280DF810 Other Parts Discussed in Thread: DS250DF810 , Hi Team,
I check below link but I would like to double check that if DS280DF810 can P2P replace DS250DF810 at hardware part, and at software part no need to change software code at <…
Part Number: DS250DF810 Other Parts Discussed in Thread: DP83869
HI there,
I hope you are well,
I have some questions regarding the correct way to connect this device inline with 2 ethernet connectors (RJ45), as if this device was in the middle of…
Part Number: DS250DF810 Hi, We have used DS250DF810 in 40G backplane application, here are 4 DS250DF810 on one board, ADDR are set to 0x30.0x32.0x34.0x36.
And we tied all DS250DF810's EN_SMB(E3) to 2V5, READ_EN_N(F13) is floating, ALL_DONE_N is floating…
Part Number: DS250DF810
Hi Team,
Could you please share the IBIS_AMI model for me? I find there is a request link in the E2E, so I also request on that. Please let me know if that method is correct. Thanks.
https://www.ti.com/drr/opn/DS250DF810-DESI…
Part Number: DS250DF810 Other Parts Discussed in Thread: DS280DF810 TI technical personnel,
Regarding the DS250DF810 and the DS 280 DF810:
What are the explicit differences?
Are they pin compatible?
Is the upper limit of the 28Gbps operation offered by…