Greetings Kenji,
DS25BR120 part to part skew refers to skew within positive and negative output of the DS25BR120 device. This normally shows itself as DCD or Duty Cycle Distortion or jitter.
On DS15EA101 this parameter is specified as total residual jitter…
Part Number: DS25BR110 Other Parts Discussed in Thread: DS25BR120 Hello,
is it possible to provide an equivalent input and output schematic for the LVDS Buffer DS25BR110 and DS25BR120? In the data sheet only a block diagram is given. To analyse the behaviour…
Part Number: TLK1221 Other Parts Discussed in Thread: DS15BA101 , DS25BR120 , DS15EA101 , DS25BR110 Dear all:
I will used two TLK1221 transmit signal between two board. Can TLK1221 transmit 5-10 meters distance with RX/TX ?
Can you help check the pull…
I will add that the DS100BR111 or DS64BR111 support SGMII in AC coupled mode. The DS25BR100, DS25BR110, and DS25BR120 will also support DC coupling with SGMII.
Regards,
Lee
Hi Arjan,
Our models have all been simulated with ADS, so I think I will not be able to view your archived project. However, if you have eye diagrams to share, that may be a way for us to see what is happening.
Using a DS25BR120 may help to give an extra…
Hi Lee,
Thank you for your comment.
In the assuming application I will use shielde twisted pair and signal groud is conneted between driver and receiver.
Do we have any issue or concerning for locating DS25BR110 next to DS25BR120 in the middle of transmission…
Part Number: DS25BR150 Other Parts Discussed in Thread: DS25BR120 , DS25BR100 , , DS25BR110 , DS90LV004 , DS15MB200 , DS25BR440 Dears,
I am looking for a LVDS buffer that support Hot Swap. But can not find a direct solution. Can you please comment and suggest…
Part Number: DS25BR110 Other Parts Discussed in Thread: DS92LV18 , DS25BR120 The DS25BR110 is being used to equalize/buffer a LVDS serdes signal after traveling over several meters of CAT5e cabling and output feeds into deserializer.
The following scope…
Other Parts Discussed in Thread: DS25BR100 , DS25BR110 , DS25BR120 , DS64BR111 Hi Team:
Do we have any part can support SGMII(1.25G) Redriver function?
Hi,
These products can work at slower speeds like 1.5 Gbps or 2.0 Gbps as well. They will have less equalization gain available at the lower frequency, but the performance is still very good.
Alternate devices for use at 1.5 and 2.0 Gbps are the
DS25…