Part Number: DS25BR440 To whom may concern,
I am using this IC as line driver for 2G LVDS signal. I test with 1.5 Meter cable and 3.8 meter cable. I Have following questions:
I tried with and without PE and EQ pin enabled, and see no difference…
Part Number: DS25BR440 Tool/software: HI,
Can I connect a LVDS interfac with SPEC:
VOH min.1.1V,
VOL Max.0.745V,
VOD_AC(transmitter differential output voltage) 390-800mV
VOD_DC (DC range for the VOD): Min.400mV
VCM (transmitter common mode…
Part Number: DS25BR440 Tool/software: Hello all,
I'm looking for the same type of buffer but >3.125Gbps and can convert SLVS-EC to LVDS.
Thanks,
Best regards,
Part Number: DS25BR440 Tool/software: Hi all,
I am investigating the DS25BR440 and the LOS pins for driving some LEDs. What is the output drive of these LOS pins? If it is insufficient to drive ~25mA of load, will I need external buffers to boost…
Part Number: DS25BR440 Hey ,
can you please tell me what is the difference between the following series :
06AHEFG3
09AKKYG3
in addition , I need the date code of both of them
thanks ,
Orel
Part Number: DS25BR440 Tool/software: Hi,
We use this component without equ/emp for LVDS
in the output pins we see a glitch (on the data and clk) like you can see in the attached picture
when we remove the component, the glitch has disappeared.…
Part Number: DS25BR440 Other Parts Discussed in Thread: DS280MB810 , SN65LVCP408 Tool/software: Dear Ti Team,
I'm looking for a LVDS BUFFER / REPEATER IC
4-data pairs and 1-clock pair.
Parameters:
5-Channel input and 5-channel output,
Data…
Part Number: DS25BR440 Hello E2E team,
My name is Takako Fujiya from Tokyo Electron Device Ltd.
Our customer requested the ESD please help to provide it.