Hi Shay,
1). I think earlier you mentioned this AC coupled? So there would be Capacitor at the transmit side of the LVDS driver.
2). What is the data rate and does this have effect on your application?
Regards, Nasser
Part Number: DS25BR440 Other Parts Discussed in Thread: DS15EA101 , DS15BA101 , LMH0384 Tool/software: Hi,
We need to use the LVDS for our design, and now, customer request the LVDS Cable is 10-15m, we test the DS25BR440 that it is only support 8m Cable distance…
Part Number: DS25BR440 Hello E2E team,
My name is Takako Fujiya from Tokyo Electron Device Ltd.
Our customer requested the ESD please help to provide it.
Part Number: DS25BR440 Hey ,
can you please tell me what is the difference between the following series :
06AHEFG3
09AKKYG3
in addition , I need the date code of both of them
thanks ,
Orel
Part Number: DS25BR440 Hi all,
I am investigating the DS25BR440TSQ/NOPB and am looking for the following parameters below. Note that I am not looking for the maximum allowable junction temperature, but for this intent and purpose I need to see what the…
Part Number: DS25BR440 Hi Team,
I hope you’re doing well! I wanted to ask about the DS25BR440 and whether there is a possibility of back feeding through this buffer if the load its driving is powered before its input side ? I was wondering if t…
Part Number: DS25BR440 Hi, support team
My customer has the questions as follow:
1. Please tell me "LOS pin is asserted when no signal is detected at input" 's specific conditions, what is identifed as "no signal"? 2. Please provide…
Part Number: DS25BR440 Hi, I would like to use DS25BR440 in my design as LVDS equalizer. From datasheet, the component performance described in the following table:
While A, B and C are different signal length in the test circuit. Few questions: 1. There…
Part Number: DS25BR440 Hi,
Could you tell me the ICC at the maximum rate of the DS25BR440.
Could you tell me the ICC of PE=ON, EQ=ON at the maximum rate of DS25BR440.
Thanks.
Part Number: DS25BR440 Hi team,
My customer have two application questions for our part DS25BR440.
Q1: External ESD diode
In our d/s, our DS25BR440 has ESD protects feature, if there is any needs customer to add external ESD diode at these I/O pins? …