Other Parts Discussed in Thread: DS25CP152 , DS90CP02 , SN65LVCP202 , SN65LVCP402 Hi,
Our customer is looking for >1.5Gbps, 2:2 crosspoint switch which have Hi-Z output when the output is disabled.
Could you please tell us if DS25CP152 have Hi-Z output…
Part Number: DS25CP152Q-Q1 Other Parts Discussed in Thread: DS25CP152 Customer is looking to use DS25CP152 to take one LVDS signal and send it to two LVDS loads.
Is it preferred to:
Feed the LVDS signal to both device inputs in parallel and have each…
Dear Nasser,
We designed the DS25CP152, but the screen appeared blue.
If you remove the DS25CP152 and connect it directly, the screen normally appears.
For the DS90UH949, the TMDS CLOCK 96Mhz is 3.36Gbps.
However, for the DS25CP152, it is a specification…
Hi Remi,
You are correct. We need 4.7uF capacitor on each pin. 4.7uF capacitor on OUT0+ and another 4.7uF capacitor on OUT0-. The other side of these two caps go to DS10CP152 device. You don't need 100-ohm resistor since this is integrated within DS25CP152…
Other Parts Discussed in Thread: DS90LV001 , DS90CP22 , DS10CP152 Hi,
We have a unit that is driving a 15 inch LVDS display at 1024 x 768 - 4 data pairs and 1 clock pair (24 bit LVDS). Sometimes we want to drive two displays with the same data. The data…