Other Parts Discussed in Thread: DS25MB100 Hello.
Obviously, the pre-emphasis parameters of the DS25MB100 have been designed for the 2.5Gbps application.
The device datasheet indicates in the introductory features list that the DS25MB100 supports 0.25Gbps…
Other Parts Discussed in Thread: DS25MB100 Hello
I have some questions about DS25MB100
If output will send two kinds of signals ,
HS mode: 200 mV (Vp-p)
LP mode: 1.2V single-end
Can DS25MB100 receive it directly ?
What is the output voltage level of the…
Other Parts Discussed in Thread: DS25MB100 Hello,
We are only using one input pair on the DS25MB100. Is it ok to leave the other input floating, or do we need to terminate it. The datasheet says it has internal terminations, but I wanted to verify that…
Other Parts Discussed in Thread: DS25MB100 , DS90UR907Q-Q1 , DS25CP102 , DS90UR908Q-Q1 I am currently designing a board that is intended to switch between two LVDS sources. The sources are from the DS90UR907. The plan is to select between two 720p video sources…
Other Parts Discussed in Thread: DS25MB100 Please advise if some one looks at this created the library then it sill problem also not provede the dimensions of DAP or GND PAD.
do you think is this the time to change the land patteren to match with Order…
Hello Vincent,
You are correct that the parallel output signal (Rx) from the TLK is TTL.
Regarding the signal from the TLK2711A to the DS25MB100.
The signal from the TLK2711A needs to be ac-coupled into the DS25MB100, and the DS25MB100 will set its own…
Other Parts Discussed in Thread: DS25MB100 Hi
She is requesting mux for two path as below.
However, the blue and magenta path will not be driven simultaneously.
I recommanded product of DS25MB100.
If you have a better solution, please recommend.
Thanks…
Other Parts Discussed in Thread: DS25MB100 Hi,
Our optical transceiver vendor has suggested to connect the SERDES interface as shown below,
For your information the Optical transceiver transmitter ports are LVPECL (DC coupled) logic. We are connecting…
Other Parts Discussed in Thread: DS25MB100 Hi,
Our optical transceiver vendor has suggested to connect the SERDES interface as shown below,
For your information the Optical transceiver transmitter ports are LVPECL (DC coupled) logic. We are connecting…