Part Number: DS26F31MQML-SP Other Parts Discussed in Thread: DS26F32MQML-SP , Hi,
Could you let me know if NAJ package of DS26F32MQML-SP and DS26F31MQML-SP?
I couldn't find 5962-7802005M2A, DS26F32ME/883 in TI.com.
Thanks.
Part Number: DS26F31MQML-SP Hello, I need SEL information for the DS26F31MQML-SP. It appears that only SEE and TID are provided on the project page. Thank you.
Part Number: DS26F31MQML-SP Hello,
I am looking at using DS26F31MQML-SP for RS422 communications. We need to be redundant and the current driver we are using has a potential issue where if one drive dies it could kill the whole chip. DS26F31MQML-SP…
Part Number: DS26F31MQML-SP Other Parts Discussed in Thread: DS26F32MQML-SP , I would like to know if the DS26F31MQML-SP and DS26F32MQML-SP have 'Cold Spare' I/O? Cold Spare simply means the I/O's are high impedance when Vcc is below a certain value or…
Part Number: DS26F31MQML-SP A few months ago I asked about the 'Cold Spare' capability of the above part number. Do all RS-422 drivers and receivers have the same feature as the Space ones? We want our RS-422 interfaces to be able to be connected to an…
Part Number: DS26F31MQML-SP
Hello,
We have seen high current consumption(approximately 30 mA) while Enable'(active low) pin is held High and Enable(active high) pin is held as high. But when Enable' is held low (While Enable pin is still held as High…
Part Number: DS26F31MQML-SP Hi Team,
Can you please advise with following request?
"
Thermal Conductivity Coefficient(W/m*K)
Thermal(Heat) Capacity(J/kg*K)
"
Thanks in advance
Best Regards
Furkan Sefiloglu
Part Number: DS26F31MQML-SP Other Parts Discussed in Thread: DS16F95
Hi Team,
Can we support on DS26F31MQML-SP with SEE, SEU, SET?
Thanks in advance
Best Regards
Furkan Sefiloglu
Part Number: DS26F31MQML-SP Hello,
I am looking for a rad hard RS422/485 driver. Some of the alternatives don’t have TID ratings in the brochure I have, so I don’t know which one to choose. Does it really matter since they are bipolar based?
I am…