Hi Daniel,
Sorry for the delay.
a. All of these patterns are DC balanced. The signal level should stay balanced for all of them. The 8b10b and PRBS7 patterns will have less low frequency content. This will decrease the maximum amplitude at the DS280 inp…
Part Number: DS280BR820 Other Parts Discussed in Thread: DS280DF810 , Hello,
We're using DS280BR820 implementing the function as below block diagram. The maximum length of the line on PCB is 1500mil. The question is there are bits-error during sending…
Part Number: DS280BR820 Other Parts Discussed in Thread: DS280MB810 , Access was granted under NDA some time ago to information for the DS280BR820 and DS280MB810, including the datasheets and programming guides, the dates of which were September and October…
Part Number: DS280BR810 Other Parts Discussed in Thread: DS280BR820 Hi,
I saw from the forum that the main difference between DS280BR810 and DS280BR820 is the coupling caps and the better equalizer gain for the 820.
But from the datasheets it seems that…
Part Number: DS100BR210 Other Parts Discussed in Thread: DS280BR820 , DS320PR810 Hello,
Does TI has auto grade re-drivers for below parts? I suppose no, would you please help double confirm? Thanks a lot.
10G: DS100BR210
25G: DS280BR820
PCIE GEN5: DS320…
Part Number: DS280BR820 Dear Sir/Ms.
About TI DS280BR820- Low Power 28 Gbps 8 Channel Linear Repeater Is this IC suitable for PCIe gen4?
Currently the customer intends to place this IC in the middle of the PCIe gen 4 ASIC to ASIC. If the DS280BR820 is not…
Part Number: DS80PCI800 Other Parts Discussed in Thread: DS280BR820 Hi team,
The IBIS model of DS80PCI800SQ/NOPB, DS280DF810ABV and DS280BR820 don't have IBIS model in ti.com. Could you tell me where I can get these parts' IBIS model? Thanks a lot!…
Part Number: DS280BR820 Hi,
We know that DS280BR820 can be used for Optical and Passive Copper (100G-SR4/LR4/CR4) application. Now we want to know if DS280BR820 can be used for 12G SDI signal transmission.
Our board is large and the line on the board is…
Part Number: DS280BR820 Other Parts Discussed in Thread: DS280MB810 , , DS160PR410 Dear Team,
May I know if this part could support SAS4 24Gbps application?
Or do we have any roadmap in the future to support SAS4?
Thank you.
Jim
Part Number: DS280BR820 Hi Team,
I got S-parameter file for TI repeater ds280br820 from TI.
I want to know that @ what Equalization values this S-parameters are extracted..
I performed simulation using s-parameters of TI repeater & other passive components…