Part Number: DS34RT5110 Other Parts Discussed in Thread: SN65DP159 , SN65DP149 , , TMDS181 , TDP0604 , TDP1204 , TMDS1204 Hi Team,
When connected through LAN cable, the communication is failed and the display of screen is not normal if the length of cable exceeds…
Other Parts Discussed in Thread: DS34RT5110 , TMDS181 Hi Team,
customer is designed DS34RT5110 on their docking board to support the 4K2K/30hz output, they feedback that the DS34RT5110 can only output the 4K2K/30hz resolution in BYPASS mode, when they set…
Other Parts Discussed in Thread: DS34RT5110 I have a question.Can DS34RT5110 support the function of HDCP? If it do not support this function,which product can replace it?
Other Parts Discussed in Thread: DS34RT5110 Looking for an HDMI interface that can support 1440p resolution. The description for the DS34RT5110 calls out the latest HDMI 1.3 and states: " The latest version, HDMI v1.3, supports a single-link bandwidth…
Hi Arseniy,
In order to provide you with the HSPICE model for the DS34RT5110, we will need to set up an NDA with you. Do you have a local TI contact that we can contact to work on this for you?
Michael
Other Parts Discussed in Thread: DS34RT5110 Hi Team,
Could you share us the power consumption data at 3.0Gbps x 3 ?
There is the information in the datasheet that power consumption is 1100mW typ. Does the power consumption decrease from this value at 3…
Other Parts Discussed in Thread: DS34RT5110 Hi Team,
I believe HDMI v1.4 would support 4Kx2K video and HDMI v1.3a does not.
However, DS34RT5110 has the maximu datarate of 3.4Gbps x3 = 10.2Gbps, the datarate which could support 4Kx2K video.
[Question] Our…
Other Parts Discussed in Thread: DS34RT5110 Hi Team,
The output pin of DS34RT5110 and the HDMI Connector pin assign is in the opposite direction. In this case you would need to use via and place the HDMI connector on the opposite side of the board.
[Question…
Other Parts Discussed in Thread: DS16EV5110 , DS34RT5110 , SN65DP159 Dear Sir:
Could you help kindly provide DS16EV5110 / DS34RT5110 / SN65DP159 EQ Gain v.s Frequency figure as follows?
If cannot, please help to provide EQ gain value on each data rate. Thanks…