Other Parts Discussed in Thread: DS38EP100 Hi,
Now we're promoting DS38EP100 to our customer and then they would like to know following parameter just for their reference.
Do you have some reference information?
1, Part to part skew
2, Accuracy…
Hi,
We do have the DS38EP100 S-parameter model, but need to insure that there is an NDA before we provide the file.
Please also let us know who is the your TI sale representative.
Regards,
Michael
Other Parts Discussed in Thread: DS38EP100 Team,
1) When using DS38EP100 on a backplane with a max trace length of 12" is there any benefit to using two of these devices - one on Rx side and one on Tx side - on each differential pair of the SGMII …
Part Number: DS100BR410 Other Parts Discussed in Thread: EQ50F100 , DS38EP100 , DS25CP102Q-Q1 , DS42BR400 , , DS100BR210 , DS100DF410 Tool/software: Hi, In the response to DS100BR410: Thermal Characteristics - Interface forum - Interface - TI E2E support…
Part Number: DS80EP100 Other Parts Discussed in Thread: DS38EP100 , EQ50F100 Hi,
I have customers who want to use this chip to drive and balance CML, because their Serdes running speed may be lower than 5G, this chip IN OUT mode, if it is lower than…
Other Parts Discussed in Thread: DS25BR150 , DS38EP100 , DS25BR101 , DS25CP104A Dear Team,
do you have a redriver, retimer, buffer or a similar IC for Sony Low voltage LVDS ( subLVDS)?
Vcm=0.9V
Vod = 150mV
Best Regards,
d.
Part Number: TLV3801 Other Parts Discussed in Thread: DS90LV001 , DS38EP100 , DS80EP100 , DS25BR110 , LMK04228 , I have a few LVDS signals coming off-board. Can I use this part to restore the eye diagram and provide very low jitter for the external LVDS…
Part Number: SN65LVCP1414 Other Parts Discussed in Thread: EQ50F100 , DS38EP100 , DS42BR400 , , DS25CP102Q-Q1 Tool/software: Hello, I'm in the process of choosing an Equaliser where I require x5 channels supporting a data rate up to 3.2Gbps. In my initial…
Hi Michael,
It's good news for me, I will try this IC(DS38EP100). Thank you!
But I found a question on PCB layout, because of some connectors pin define limited, if the differential positive pin has to connect to IOA+ of DS38EP100, the negative pin…
Hi Gokul,
Can we use this Passive Power-Saver Equalizer DS38EP100 ?
Is there any IC that work at rate of 10\100Mbps ?
Compatible to PHY ethernet DP83826E ?
Regards,
Meir