Part Number: DS50PCI402 I think i understand how this part works in general, i'll make some statements, please tell me where i'm wrong, or there is some nuance which i should consider.
the DEMx[1:0] pins control the Vod and De-emphasis, which affect…
Part Number: DS50PCI402 Hi team,
Could you please let me know how to modify the VOD settings?
Registers only provide 4 fixed values, what should I do if I need other values?
-------------------------- 03'h = 600 mV (Default) 07'h = 800 mV 0F'h …
Part Number: DS50PCI402
Dear Technical Support Team,
I have been trying following issue.
e2e.ti.com/.../930604
I tried various settings, but there was no combination to solve link up issue. It is NG even in Bypass mode.
Therefore, when DS50PCI402…
Part Number: DS50PCI402 Dear Technical Support Team,
According to the datasheet, Return loss specs such as RLRX-DIFF and RLRX-CM show minus dB(-21dB,-20dB,-11.5dB).
I think that the Return loss shows plus dB. If minus dB is correct, could you inform…
Part Number: SN65LVPE504 Other Parts Discussed in Thread: DS50PCI402 , Hi
The situation I encountered was a PCIe root port with X8 GEN3 signal, and the downstream device had X4 GEN2 bandwidth. We found that sometimes the device can only recognize the…
Part Number: DS50PCI402 Other Parts Discussed in Thread: DS50PCI401 , Hi team.
Thank you for your usual support.
I am suffering from device selection.
I think [DS50PCI401] and [DS50PCI402] seem to have the same characteristics.
Whis is your…
Part Number: DS50PCI402 Dear Technical Support Team,
I have a question about DS50PCI402.
The chapter "Power Supply Bypassing"on page 30 of datasheet shows below and it said "three capacitors with capacitance in the range of 2.2 μF to 10 μF ".
In…
Part Number: DS50PCI402
Dear Technical Support Team,
My application is using backplane with PCI402.
If only AC coupling on the RX side of the endpoint of the backplane is changed to 0Ω resistance Link up now works properly. (Red circle )
If…
Other Parts Discussed in Thread: DS50PCI402 Hello,
Our customer use the DS50PCI402.
It is mentioned 'Output will test for the presence of receiver input every 12ms' on the datasheet.
How about the variation of this time (12ms) due to the process…