Part Number: DS90C385A Other Parts Discussed in Thread: SN75LVDS83B , SN65LVDS93B-Q1 , DS90C3201 Is there p2p compatible one with THC63LVDM83D (Thine)?
Thanks.
Regards
Brian
Part Number: DS90C3201 Other Parts Discussed in Thread: DS90C387A , , CDCS501 I have a question regarding DVI to LVDS conversion.
In the SLLA325A application sheet it is recommended to use the DS90C387A for Dual Pixel application. But since we would like…
Other Parts Discussed in Thread: DS90C3201 , DS90C387 , DS90C387A , DS90C187 , DS90C3202 , DS90CR485 , DS90C387R , HD3SS213 , TFP401A I'm comparing the DS90C3201 with the DS90C387/A parts and have some questions.
DS90C3201, 3.3V 8 MHz to 135 MHz Dual FPD-Link…
Other Parts Discussed in Thread: DS90C3201 , DS90C3202 , DS90CR483 INTEL are looking for interface device to transfer parallel I/O to serial cable (DP,HDMI).
From looking at TI website they found two devices that may fit :.
For transmit : DS90C3201
For receive…
Other Parts Discussed in Thread: SN75LVDS83B , DS90C3201 , SN74AVC32T245
Since the National acquisition is finalized, I assume that it is OK to ask about this part in these forums now. I need a LVDS transmitter to go from an OMAP (OMAP4430/60) to a dual…
Other Parts Discussed in Thread: DS90C3201 , TFP401A , DS90C387A , TFP401 , DS90C187 , DS90C387 Hello,
I'm currently designing a monitor solution for HDMI/DVI (no audio). I would have to support both 1280x800 pixel single-link LVDS display and 1920x1080 pixel…
Hi Phil,
The DS90C3201 is a serializer that converts 3 x 10 RGB color depth into its corresponding OpenLDI LVDS output (in this case, there would need to be 5 x LVDS data pairs and 1 LVDS clock). However, the DS90C3201 only supports RGB inputs for single…
Other Parts Discussed in Thread: DS90C3201 Hi,
I'm looking for a solution to converter RGB from a LCD to LVDS. It should support 12/16/18/24 bit RGB. I'm looking at DS90C3201, but I don't think it support more than 12 bit.
Thanks.
Hi Nat,
The DS90C3201 and DS90C3202 are the highest performance devices we have in the 10-bit per pixel range. The maximum clock speed for these devices is 135 MHz.
Regards,
Lee
Other Parts Discussed in Thread: DS90C3201 , SN65LVDS822 Hi,
The datasheet says the transmitter runs from 18 to 87.5 MHz and the receiver runs from 20 to 85 MHz. We already have the transmitter built in and drive an SVGA display at ~30 MHz. This works fine…