Part Number: DS90CF384A Other Parts Discussed in Thread: DS90CF364A , , DS90CF364 Hi,
Customer of mine intend to use DS90CF384A to convert 18bit RGB TFT panel, Can this be done or I should consider DS90CF364A or DS90CF364 ?
Please refer below circuit connection…
Part Number: DS90CF384A Other Parts Discussed in Thread: DS90CF364A Hi,
We're trying to drive a two low resolution LCD displays, 480 x 270, and the maximum pix clock frequency of the display is 10.99 MHz. The interface has to be LVDS to RGB, but the only…
Hi Kato-san,
It should be okay as long as the YCbCr data is within specification of the datasheet parameters. It doesn't look like the LVDS302 does much with the data except deserialize it. Any unused LVDS inputs can be left open.
Is there a particular…
Other Parts Discussed in Thread: DS90CF364 , FLINK3V8BT-85 , DS90CF364A , SN75LVDS86A Hi
I'm interested with DS90CF364 EVM.
According to the web, the EVM would be FLINK3V8BT-85/NOPB.
However the chipset inside is
One Transmitter board with the DS90C385MTD…