Part Number: DS90LV004 We have a setup where there’s a chance this part could be powered off while the FPGA driving it could be powered on. Is there any information on if this will cause the board VCC plane to be powered up in this case? We have the enable…
Part Number: DS90LV004 Dears:
Could you kindly help to check the schematic, since we found the temperature of DS90LV004 is so high(about 60˚C) on the welded board and FPGA dose not run any program code.
Is it normal? And pls. kindly help to give some…
Part Number: DS90LV004 Datasheet P6 is described about internal termination and I have a question for Figure 6.
Figure 6 termination is connecting 100Ω both Driver(internal) side and Receiver side.
Is this mean signal amplitude become half because…
Part Number: DS90LV004 Hello to whom it may concern,
Could you please refer to the following questions for the PN: DS90LV004?
1. Could you please tell me the value of the operating Junction Temperature(TJ)?
2. If there is no data of Tj, could you…
Part Number: DS90LV004 Hi Team,
I'm looking for a device that can drive a high number of LVDS lanes (up to 14 lanes), each with a signaling rate of 800Mbps. The goal is to transmit this data from one board to another through a 10m cable. So, this leads…
Hi,
Can you please refer to the following questions for the PN: DS90LV004TVS:
May I assume that the inverting and non-inverting inputs of each channel are interchangeable? Meaning, can I input the ‘P’ signal to the inverting inputs and the ‘N’ signal…
Part Number: DS90LV004 Dear, Sir
This is Joong-hyeok Lee, DMSMS researcher of Leoinnovision. Leoinnovision is the official EOL(End Of-Life)/obsolescence part manager of Korean Military (Army, Navy, Air force) and PLM agency of many defense industries …
Part Number: DS90LV004 Other Parts Discussed in Thread: DS90LV001 , , DS25BR110 I need to connect two board with LVDS signal. The distance between these two boads is 6 meters. I want two use DS90LV001 as the buffer on the receiver board. But I am worried…
Part Number: DS90LV004 Other Parts Discussed in Thread: DS15BR400 , DS25BR440 , DS100BR410 Part to Part Skew for the DS90LV004 is 1.1ns
we need to select similar part but offering less than 100ps on part to part skew feature, what do you recommend?
As many…
Other Parts Discussed in Thread: DS90LV004 Hello
I have a question about the DS90LV004TVS/NOPB device.
In my system there are two boards. The DS90LV004 is configured as a LVDS receiver. Under certain circumstances, the board with the DS90LV004 will be…