Part Number: DS90LV032ADS90LV032A is fail safe to high with no input, terminated input or shorted inputs IAW datasheet 8.3.1. Is there any way to change the fail safe condition to low for no input or terminated input with external resistors and an external…
Part Number: DS90LV032A Should serial resistive terminators be required for the interface circuits as shown in the attachment? Thanks
serialTerminators.docx
Part Number: DS90LV032A
Hello,
I am designing a circuit that uses DS90LV032A.
Now caluculate power consumption of the DS90LV032A.
I would like to confirm the input capacitance value of the DS90LV032A RIN+ / RIN- input to caluculate the power consumption…
Part Number: DS90LV031A Other Parts Discussed in Thread: DS90LV032A , TPD1E1B04 Hello,
I am designing 50Mbps LVDS interface cricuit. DS90LV031A and DS90LV032A are used to this LVDS interface circuit.
And I will add protection diodes to DS90LV031A…
Hi Lee,
Attached are two scopes.
SCR50 shows the supply rail powering up (3.3V; “C4”); C2 is the a 5V rail used for triggering the scope. The 3V3 rail power-up takes about 4 milliseconds.
SCR51 shows the same 5V rail for triggering, and two different…
Part Number: DS90LV031A Other Parts Discussed in Thread: DS90LV032A Hello, My customer plans to use DS90LV031A and DS90LV032A to transmit and receive 12.624Mbps CMI (Code Mark Inversion) code data having only ac component via 100ohms/0.5m differential…