Part Number: DS90LV048A Hello experts,
Please tell me the following.
Is it OK to connect LED at ROUT of DS90LV048A?
I want to drive Case 1 or Case 2 of the attached circuit with ROUT output.
LED current will be 10mA max.
Best regards,
Sakai
Part Number: DS90LV048A Hi team,
Is it OK to connect LED at ROUT of DS90LV048A?
ROUT will be connected to LV047A as well. Polarity is TBD.
LED current will be 10mA max.
Best regards,
Itoh
Hi Daniel,
Table 1 in the datasheet shows that you will have to actively drive the input signal such that VID < -0.1V in order for the output to be low.
Please refer to this post with another interested in this application: DS90LV048A: Output LOW on…
Part Number: DS90LV048A Team,
I need help on to bias the input of DS90LV048A, pin 1 and 2 so the output pin 15 to be at logic low.
Right now I have 75 ohms resistor connects between ground and pin 2 of U93 and 155 ohms resistor connects between +3.3V…
Part Number: DS90LV048A Hi team,
Please tell me the following.
What are the maximum IOL and IOH values of the DS90LV048A output (ROUT)?
Best regards,
Sakai
Part Number: DS90LV048A Other Parts Discussed in Thread: DS90LV047A , SN65MLVD047 , SN65LVDS047 recently we have witnessed some lvds data transfer problems between boards on our multidrop backplane. The design dates to before mlvds so just uses a single…
Other Parts Discussed in Thread: DS90LV048A , SN65LVDS4 Good day,
I would just like to enquire as to whether the DS90LV048A supports all LVDS voltage standards i.e. 3.3V LVDs, 2.5V LVDS, 1.8V LVDS.
Thank you for your time,
Regards,
Luke
Part Number: DSLVDS1047 Other Parts Discussed in Thread: DS90LV048A , , DS90LV047A , DSLVDS1048 Hello team,
What is the difference between DSLVDS1047 & DSLVDS1048 vs DS90LV047A & DS90LV048A?
My customer may like cost effective new parts, but do DSLVDS1047…
Part Number: DS90LV048A Hello guys,
One of my customers is looking for a conversion device which can convert from HDMI to I2S.
I think DS90LV048A could be used for HDMI -> I2S converting.
Can this device used for conversion from HDMI to I2S?
Your reply…