Part Number: DS90UB913A-Q1 One of my customer currently uses the DS90UB913 / 914 in several of their designs with a line rate of 1.344 Gbps and has following questions: We transmit the FPD-Link III signal over standard Cat-6 Ethernet cables, up to about…
Part Number: DS90UB913A-Q1 Hi Team,
Following up from my previous post (e2e.ti.com/.../ds90ub913a-q1-register-behavior
To test the clear logic, interested in knowing how, if possible, to inject these errors manually (through register writes or some other…
Part Number: DS90UB913A-Q1 Hi Team,
I have a question regarding Figure 8-1. Suggested Power-Up Sequencing.
It is mentioned that a bit error may occur when the t3 Max condition of 16ms is not met.
If PDB is asserted after the t3 provision, will the bit…
Part Number: DS90UB913A-Q1 Dear sir,
Just said in the topic, How to distinguish DS90UB913 from DS90UB953? Is the device id used for this purpose?
Best regards
David
Part Number: DS90UB913A-Q1 Hi Team,
Couple of general register behavior questions I have, hopefully you can help clarify my understanding for these:
Is the CRC error counter in registers 0x0A and 0x0B cleared by writing to ERROR RESET in register 0x03…
Part Number: DS90UB913A-Q1 Hey Team,
Could you share details of what criteria the 913 looks for to flip the PCLK Detect bit to 1:
I have a troubleshooting situation where we are getting 0x13 for register 0x0C so we are getting a lock but no PCLK so wanted…
Part Number: DS90UB933-Q1 Other Parts Discussed in Thread: DS90UB913A-Q1 , How do I determine if the DS90UB933-Q1 or DS90UB913A-Q1 device is operating in RAW10, RAW12LF, or RAW12HF through registers?
Part Number: DS90UB914A-Q1 Other Parts Discussed in Thread: DS90UB913A-Q1 ,
The DS90UB913A-Q1 catches ACK during I2C communication. However, ACK is not output from a DS90UB914A-Q1 .
This phenomenon occurs only with a specific address, and normalcy works…
Part Number: DS90UB913A-Q1 Hi all,
I have a small problem regarding the FPD-LINK,
I don't understand how can I calculate to max camera sensor size that i can have as an input to the serialize.
what are the main factors that i need to consider?
thanks…
Part Number: DS90UB913A-Q1 Hello Team
My customer has idea to implement as below for function test line.
They use Coax cable and POC will be implemented at MUX side after AC coupling cap.
if this idea is possible, they believe 1ea 964 board can do test…