Part Number: DS90UB913A-Q1 If we want to run the 913A's i2c with fast mode(400khz), what’s the settings needed on 913/960. Is the below correct?
Should configuration of UB913 for register 0x11/0x12 SCL High/Low time be set to 0x19 for 400 KHz?
…
Part Number: DS90UB913A-Q1 Hi,
For a RAW-12 based camera which has DS90UB913A, we are interfacing it to a processor through DS90UB960 Deserializer. What we see is, the Sensor is outputting(checked by probing through scope) the PCLK and other Sync and…
Part Number: DS90UB913A-Q1 Hi,
For a RAW-12 based camera which has DS90UB913A, we are interfacing it to a processor through DS90UB960 Deserializer. What we see is, the Sensor is outputting(checked by probing through scope) the PCLK and other Sync and…
Part Number: DS90UB913A-Q1 Other Parts Discussed in Thread: DS90UB936-Q1 , DS90UB925Q-Q1 , DS90UR910-Q1 Hi,
Good Day. I have a customer who needs a converter IC which has to convert parallel 10 bit video data to MIPI-CSI2 interface.
I found a solution in…
Part Number: DS90UB913A-Q1 Hi team, I'd like to know about setting R3 for IDXpin. R3 is set to 10kΩ to set address 7. However, it changed to OPEN due to the revision change of the datasheet. Is there a problem with R3 set to 10kΩ? Sincerely…
Part Number: DS90UB933-Q1 Other Parts Discussed in Thread: DS90UB913A-Q1 , Hi whom it concerns,
I would confirm both DS90UB933-Q1 and DS90UB913A-Q1 as below points
1. These parts electrocal and internal block are same,right?
2. The external connnection is…
Part Number: DS90UB913A-Q1 Other Parts Discussed in Thread: DS90UB913A-CXEVM , DS90UB914A-CXEVM Hi, We about to end the layout this week and the layout person just highlight something regarding thermal pad connection, so we need your feedback ASAP.
In DS90UB913…
Part Number: DS90UB913A-Q1 Hello team,
My customer is checking if other inductor can be used for POC to have dual supplier source.(this project is on MP)
current inductor(L16 in picture) solution is TDK ADL3225V-470MT-TL000.
but now they are considering…
Part Number: DS90UB913A-Q1 Hi, Team,
How should I understand this description?
"does not auto update IDX strapped address"
I understand the device ID is set by Strap when PDB goes High timing, and the value is auto loaded into the 0x00[7:1…
Part Number: DS90UB913A-Q1 Hello~!
Please help me.
I'm developing a 1 megapixel camera.
The LVDS PoC output is being used using DS90UB913.
There was a problem with the image shaking during ESD TEST, so you want to apply D2 (V2AF118A400Y2E) to the…