Part Number: DS90UB962-Q1 Tool/software: Hi team,
The customer uses 933-962. 933 is powered on and initialized by the APA SOC, while 962 is initialized by the Head unit SOC. I want to confirm whether there is a necessary order for the initialization of…
Part Number: DS90UB962-Q1 Other Parts Discussed in Thread: DS90UB933-Q1 Tool/software: Hello TI experts,
In our project we have four cameras connected to the ds90ub962 Deserializer,and we found that some times there are one of camera cannot be locked…
Part Number: DS90UB962-Q1 Hi team,
could you help with this problem, please refer to the below E2E
https://e2e.ti.com/support/interface-group/interface---internal/f/interface---internal-forum/1353029/ds90ub962-q1-how-to-close-signal-on-csi-2-port-1
customer…
Part Number: DS90UB962-Q1 Hi team,
support four channels analog high definition camera input(CVBS input).
support analog high definition AHD or TVI camera input.
The customer requirement is as the above description, I want to know if the need match …
Part Number: DS90UB962-Q1 1. The camera uses 953 2lane 1920x1080 and the data format is yuyv 25fps. Can Ub962 support four cameras simultaneously? How many cameras does ub962 support in terms of bandwidth? 2. The camera adopts 953 4lane 1920x1080 and the…
Part Number: DS90UB962-Q1
Hi FPD Link Team,
My customer are designing AVM system and set UB933 for output, and IVI receiver is UB962. Besides, the IVI system has been RTM couldn't make change any more.
Here is UB962 Raw 10 8-bit register configure…
Part Number: DS90UB962-Q1 Hi team,
The RVC lens uses a 962 deserializer, which requires a FrameSync signal for the lens to produce pictures;
The following is the FrameSync settings in the 962 datasheet. I measured the waveform according to this configuration…
Part Number: DS90UB962-Q1 Hello friends,
If we set LV_POLARITY and PV_POLARITY as 0 in UB962 and we pull down HSYNC and VSYNC in UB933, is it OK?
Do we have soft configuration in UB933 to change the status of the HSYNC and VSYNC?
Best Regards
Yuan …
Part Number: DS90UB962-Q1 Other Parts Discussed in Thread: DS90UB935-Q1 , DS90UB953-Q1 The changes in the camera aspect of the new project compared to the old project are as follows:
1. The resolution has changed from 1920 * 720 to 1920 * 1440
2. The serializer…