Part Number: DS90UB962-Q1 Regarding FrameSync configurations based on the Deserializer ub962 and Serializer ub953 Datasheets:
I have the following understanding:
If DeSer 962 and Ser 953 (in camera) are in Synchronous mode, then FrameSync is directly…
Part Number: DS90UB962-Q1 Hello,
One customer used DS90UB962 for their automotive application. He need to set up 30MHz frame sync with cameras connected DS90UB933. The frame sync mode is basic synchronized forwarding mode, and 0x21=0x14. Now the GPIO1…
Part Number: DS90UB962-Q1 Hi Team,
I'm working on a debug effort with my customer. We are looking at the mode strap table and have a few clarifications:
1. Strap NO 0 in the above table seems to make the device run in nonsync mode. Is this expected…
Part Number: DS90UB962-Q1 Hello,
One customer uses DS90UB962-Q1 for EMC test,, which shows a 1600MHz frequency overrun during whole-unit EMC re testing.As to the UB962, the high 1600MHz frequency point can also be detected from the 962 chip itself…
Part Number: DS90UB962-Q1 Other Parts Discussed in Thread: DS90UB960-Q1 , What's the difference bettween DS90UB962-Q1 & DS90UB960-Q1 in hardware design?
Can DS90UB960-Q1 external circuit compatibility with DS90UB962-Q1's external circuit if use…
Part Number: DS90UB953-Q1 Other Parts Discussed in Thread: DS90UB964-Q1 , DS90UB936-Q1 , DS90UB962-Q1 , DS90UB954-Q1 , DS90UB960-Q1 , DS90UB934-Q1 , DS90UB914A-Q1 , DS90UB9702-Q1 As per datasheet DS90UB953-Q1 is compatible with DS90UB954-Q1, DS90UB964-Q1, DS90UB962…
Part Number: DS90UB962-Q1 Hello,
The four cameras connected DS90UB962 could appear jam phenomenon. And the customer has tried all the boards have the same problem. Please refer to the below video. Do you have any suggestions? If is there any registers…
Part Number: DS90UB962-Q1 Other Parts Discussed in Thread: DS90UB964-Q1 , Dear expert,
If I solder DS90UB962-Q1 silicon to DS90UB964-Q1 EVM, does it work?
Thanks
Part Number: DS90UB962-Q1
Hi Team,
There is a good new that we DIN DS90UB962-Q1!
But there are currently issue that need to be resolved
The video is the synchronized waveform when 2, 3 and 4 are lit At present, there are measurement cameras at this time…
Part Number: DS90UB962-Q1 Hi team,
Power up sequence is described in the datasheet 9.2 Power-Up Sequencing, but I could not find the timing requirement between VDD18 and VDDIO.
In my setting, VDDIO=3.3V.
1. Power up sequence
Is it OK to power up like…