Part Number: SN65LVDS3487 Other Parts Discussed in Thread: DSLVDS1001 SN65LVDS3487 vs dslvds1001
Hi,
I am Stuck in a issue where i used dslvds1001 in place of SN65LVDS3487, because of which the counter reciever stopped responding
Can you please guide me…
Part Number: SN65LVDS4 Other Parts Discussed in Thread: DSLVDS1001 Dear Anyiam,
please can you confirm that we can connect DSLVDS1001 to SN65LVDS4 when VCC and VDD of SN65LVDS4 are powered with 1.8V ?
Best Regards,
d.
Part Number: DSLVDS1001
Hello,
We are having a Serdes interface which requires a reference differential clock 101MHz with maximum jitter +/-10ps (Peak to Peak Jitter) . The single ended clock source with low jitter/phase noise spec is identified, however…
Part Number: SN65MLVD2 Other Parts Discussed in Thread: DSLVDS1001 Hi Expert,
Good day.
We have these queries from client regarding two parts the SN65MLVD2- Single channel M-LVDS type-1 receiver and the DSLVDS1001 400-Mbps, Single-Channel LVDS Driver what…
Part Number: DSLVDS1001 Hi,
Good Day. In the event the input of the DSLVDS1001 is a tri-state condition, what is the output of the DSLVDS1001? Thank you very much.
Best Regards,
Ray Vincent
Part Number: DSLVDS1001 Other Parts Discussed in Thread: DS90LV011A Hi team,
My customer is evaluating DSLVDS1001, and he found that this device is non-RoHS, do we have a plan to make it meet RoHS?
Best,
Zeming
Part Number: DSLVDS1001 Other Parts Discussed in Thread: SN74AXCH1T45 Dear *,
we have to generate 100MHz clk from single ended clk to differential clk.
we came across DSLVS1001 and it has good LVDS output 1.25V ± 350mV but then input high voltage min…
Part Number: DSLVDS1001 Other Parts Discussed in Thread: DSLVDS1002 , Hi team,
why the DSLVDS1001 and DSLVDS1002 ESD performance are not the same?
The ESD is for all I/O pins, no matter single end and differential pins, right?
Thanks.