Part Number: ESD122 Other Parts Discussed in Thread: TPD4E02B04 Hi,
I'm finding ESD diode that spec compatible with NXP PUSB3FR4. Is there any ESD diode from TI that support DP 1.4 & have I/O-to-GND Capacitance =<0.35pF?
Thanks,
Alice
Other Parts Discussed in Thread: ESD122 , ESDS302 , TPD2E1B06 , TPD2E007 Hi,
I am looking for replacements that has a package larger than ESD122DMXR and TPD2E007DCKR.
These parts are too small to mass-produce.
ESD122DMXR is used for USB and LVDS.
TPD2E007DCKR…
Part Number: ESD122 As per the datasheet you have already mentioned that this part is suitable for PCIe interface. But you are not provided any reference diagrams for PCIe application. what are the key points to be considered while providing ESD protection…
Part Number: ESD122 Tool/software: WEBENCH® Design Tools Is there an S-parameter model available for the ESD122? I need this for system-level simulations
thanks,
-Shriram
Back to Interface Home Page
DisplayPort Protection
Highlights:
Data speeds up to 20Gbps
8 data lines, 20 total pins
3.3V, 500mA Input
Low capacitance required on data lines
Device
V RWM
Cap
(pF)
ESD(kV)
IEC61000-4-2
Contact
No. of Chan…
Part Number: ESD122
Hello
I am planning to use ESD122DMXR to protect cJTAG pins( MCU operation 3V) because of small size.
Please confirm we can use this or suggest dual channel smallest possible protection diodes.
Thanks,
Raghu
Back to Interface Home Page
UART Protection
Highlights:
Lower speed serial data transfer interface
Operating lines: GND, ±TX, ±RX
Datalines (±Tx, ±Rx) Operating voltage: 3.3V, recommended Vbr > 3.6V
Data rates up to 5…
Back to Interface Home Page
PCIe Protection
Highlights:
PCIe: High speed serial bus expansion standard
Slots come in different sizes: x1, x4, x8, x16, x32, x64
Each lane has two differential signaling pairs (Tx, Rx)
PCIe Gen 5 bandwidth: 3.94Gbps per…
Part Number: ESD122 Other Parts Discussed in Thread: TPD4E02B04 , TDP142 ESD team,
Can you confirm if the ESD122 can be used for DisplayPort 1.4? I believe it should be fine since the datasheet says it supports DisplayPort 1.3, which has the same data…