Part Number: ESDS311 Other Parts Discussed in Thread: TIDA-010242 Hi All,
How many levels of IEC61000-4-5 has been tested for ESDS311? Please tell me the level of IEC61000-4-5.
Also, are there any other surge protection diode arrays that can provide…
Part Number: ESDS311 Other Parts Discussed in Thread: ESDS312 , STRIKE Tool/software: I started a discussion over in the Audio forum about ESD protection on the mic inputs. They suggested I try again over here. Is there any ESD device I can put on the…
Part Number: ESDS302 Other Parts Discussed in Thread: ESDS311 Tool/software: I am looking for SPICE model for ESDS302/ ESDS311 or any of the similar ESD device which can be used for the Ethernet Surge protection.
Thanks
Part Number: XTR117 Other Parts Discussed in Thread: TLV333 , ESD321 , ESDS311 , INA219 Tool/software: Dear E2E Team,
I'm trying to get a 4-20mA receiver circuit with analog output in the 0-3V3 range and I found a suggestion from 4 years ago, in a reply…
Part Number: ESD204 Other Parts Discussed in Thread: TPD4E02B04 , STRIKE , ESDS311 Tool/software: Hello,
Last year I created this forum post:
ESD204: Utilization on I/O Detection Circuit as Well as I2C
I have a couple additional questions/comments…
Hi Billy,
Yes, R1 to MCU Port , TVS to GND, R2 to connector pin. So R1 will limit the peak current going into the MCU. I don't think this would compromise the logic levels, but there is a chance the signals will slow down.
If you are willing to increase…
Hi Dean,
I checked with some other colleagues and due to the low voltage limit, you might be better off relying on the protection already provided by the device.
However if you want to get in touch with the ESD diodes team about some solutions, you…
Hi,
Would you like the replacement to be pin 2 pin or is that not necessary? For p2p, our best cross would be ESDS311 which comes in SOD323 and has similar specs to GBLC03I but the capacitance is higher. If a lower capacitance is required then the replacement…
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation…
Back to Interface Home Page
Ethernet Protection
Highlights:
10 Mhz to 125 Mhz (10Mbps to 1Gbps)
Operating line voltage ranges from -3.1 to 3.1V
Recommended capacitance < 5 pF
TI Products Recommendations
Working Voltage…